STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC does not output intended values

This should be easy but somehow I cannot make it work? I am working with the ADC of my STM23F4 Board trying to read the input from an AC voltage sensor. My previous code was using HAL and it was outputting my desired values (around 2000), but when I ...

Resolved! STM32L4P5RG two OSPI with multiplexed pin not working

Hi :I have a custom board, the mcu is STM32L4P5RG, I also connect Flash W25Q128(OSPI1) and APS6404L(OSPI2) to it.But I can't reset them and hal status always return HAL_ERROR. Can someone help me?The hardware schematic(Sch.png),Clock configuration(Cl...

Sch.png Clock.png OSPI1.png OSPI2.png

Resolved! CAN Frame Repeating, but is received

Summary: I'm seeing a situation where the CAN frames are repeating when they should only be sent once.  However, the receiving device is receiving them just fine.  Details:I'm running an STM32U545 on it's Nucleo Board, and using a simple CAN transcei...

sethkaz by Associate III
  • 13816 Views
  • 18 replies
  • 1 kudos

Custom linker file for bootloader stm32f429

Hi amazing community..I have developed a custom linker file for stm32f429. Here there is my costum linker file   /* ****************************************************************************** ** ** @file : LinkerScript.ld ** ** @author ...

SGasp1_0-1715950755530.png SGasp1_1-1715950903795.png
SGasp.1 by Senior
  • 8780 Views
  • 18 replies
  • 1 kudos

STM32H573I-DK stuck in EMW3080 firmware update utility

Hello,I have a STM32H573I-DK and I tried to update the firmware of X-WIFI-EMW3080B as described in the package "WiFi firmware update for MXCHIP EMW3080B on STM32 boards" downloaded from https://www.st.com/en/development-tools/x-wifi-emw3080b.html#st_...

jmub by Associate
  • 2370 Views
  • 3 replies
  • 1 kudos

Resolved! HAL_UART_Receive() not working correctly.

Hey, I'm using STM32F303RET6 and need to implement UART communication via USART1 (PA9 as Tx and PA10 as Rx).I managed to print "Hello World" on my console,Which means Tx is working fine and my console is configured correctly, but couldn't receive byt...

0693W000001siC3QAI.png
RLosc.1 by Associate II
  • 12726 Views
  • 7 replies
  • 0 kudos

SPI doesn't work with PDM mic

Hello guys, I'm testing a PDM mic with the nucleo-h723gz to capture in polling mode. Now I tested it with the I2S peripheral and I don't have any problem at all. But when i try to use the SPI I don't get any data: my buffer remain empty and the regis...

_legacyfs_online_stmicro_images_0693W00000FBzkg.png
LLavr.1 by Associate II
  • 2749 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.