STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Touchscreen HMI solution

Hello,Does ST mirco provide a readmade Touchscreen HMI solution which can be interfaced with an existing system and display inputs received through the exisiting system on the display with minimum modifications, should be easily configurable and adap...

ATank.1 by Associate III
  • 1005 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L496 Missing Bits in SVD-File

Hi,I just downloaded "STM32L496.svd" (Version 1.3) from ST homepage and noticed that there are missing bits in register definitions:CCMR1:Bit 16 -  OC1M[3]Bit 24 - OC2M[3]CCMR2:Bit 16 -  OC3M[3]Bit 24 - OC4M[3] 

Resolved! Limitation of SPI3 of STM32U5

I spent many hours trying to make the SPI3 works through the use of the HAL but it was doing weird things (not clearing IRQ flag so ISR was continuously called).Then I found that SPI3 is limited to a size of 1023.I also found on this forum other peop...

nicolas by Senior II
  • 1458 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-MKI109V3 unresponsive after firmware update

I have an STEVAL-MKI109V3 and the MKI238AA evaluation boards.I was unable to communicate with the MKI238AA with the UNICO-GUI software so I updated the firmware on the MKI109 with the ProfiMEMSToolV3.60.7 .bin file using the STM32CubeProgrammer follo...

lylefw by Associate
  • 4902 Views
  • 5 replies
  • 2 kudos

Clock cycle shift on GPIO output STM32F103

Dear Community,I am porting an old application made on AVR to STM32, and I am facing a strange timing issue. In a nutshell, the application is reading sector (512 Bytes) from a SDCARD and output the content of the buffer to GPIO with 4us cycle (meani...

Screenshot 2024-05-12 at 06.30.59.png Screenshot 2024-05-12 at 06.32.34.png
vbesson by Senior
  • 26683 Views
  • 40 replies
  • 3 kudos

STM32 Timer 8 ETR pin behaving as output

Hello Team,I am using an STM32F469NIH6 in my project and the following is my use case: I need the timer 8 to act as a slave to its ETR pin, which is PA0. I have a signal coming out on the PG7 from my daughter board and I have connected PG7 and PA0 vi...

Jansunil_1-1716800431150.png Jansunil_2-1716800447179.png
Jansunil by Associate II
  • 2701 Views
  • 4 replies
  • 0 kudos

Resolved! SMBus on STM32C031

Hi ST tesam,When I use  HAL_SMBUS_Master_Receive_IT( ) to receive data from device ,I can not got the information directly after the HAL_SMBUS_MasterRxCpltCallback( SMBUS_HandleTypeDef *hsmbus ) was complete.(I had set a flag when HAL_SMBUS_MasterRxC...

LsnLeeJW by Associate II
  • 3387 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 downstream of a USB hub

Hi !An application I am working on has a PC connecting to an ethernet device (currently through Ethernet) and a STM32 (STM32G0B0CET6) through USB.I am looking to only have one connection to the PC through USB, hence I am looking to have the incoming ...

4lch by Associate II
  • 2677 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.