STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware update - STM32F756 Internal / QSPI

I have board using a STM32F756 that I need to update the firmware from internal flash. I am  able to copy .bin file from an external  flash to internal flash  (Using QSPI).  I do NOT want to execute the code from the external location. It is just a t...

Resolved! Can't run EXTI on Nucleo65-H503

Hello! I'm following the STM32 tutorial on External interrupts from here and got stuck. The controller doesn't react to the press of button and the IDE for some reason switched to tab of `startup_stm32h503rbtx.s`. Reproducing steps:1. Create a new pr...

Resolved! Nucleo-F439ZI internal temperature sensor

HI team,I am working in NUCLEO-F439ZI board, now I am doing multi-channel ADC, in that I selected ADC 1 for getting the data, in ADC1 select CH3 and CH10 and Internal Temperature sensor. The data from CH3 and 10 work fine, but the internal temperatur...

STM32U585 RTC DST

HII use the STM32U585 with HALThis is my setting for time :_sTime.Minutes =_minute;_sTime.Seconds =_seconde;_sTime.TimeFormat =RTC_HOURFORMAT_24;_sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; if (HAL_RTC_SetTime(&hrtc, &_sTime, RTC_FORMAT_BIN) != H...

Markko67 by Associate II
  • 771 Views
  • 0 replies
  • 0 kudos

Resolved! Address jump function

Hi, in my project I am try to jump 0x8002000 address . but I am facing some failure, typedef void (*FunctionPointer)(void); // Example function to jump to another addressvoid jumpToAddress(uint32_t * address) { //address =0x800029c;    // Define a fu...

NandhakumarGanesan_0-1716892537128.png NandhakumarGanesan_1-1716892659863.png

STM32H7 Dual Core ADC/DMA "locking"

I have a setup on a dual core STM32H755 device with each core measuring two ADC channels with shared pins at different sample rates. The M7 core measures ADC1 Ch15 and Ch5 at 1MHz@14bit, with a sampling time of 1.5cycles (20MHz ADC clock prescaled by...

IrisDM_0-1706283076021.png
Iris-DM by Associate III
  • 4133 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.