STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC SRAM not working

Hello,We have been using two SRAMs (CY7C1061G30-10BV1XE) & one NAND Flash(MT29F8G08ADAFAH4-AAT) interfaced with STM32L562 micro-controller on same FMC bus. We have initialised FMC and try to access SRAM1 by selecting Chip select: NE1 and Bank 1. It i...

ashutoshtekriwal_0-1716960220488.png

Resolved! Portability of the code STM32F411

 Hi,I have built a program on my Nucleo F411 development kit, which has an STM32F411RE on it. I want to design a custom PCB for my program and use the same STM32F411, but this time in an STM32F411CE format.Using STM32CubeIDE, would it be possible to ...

DRous.1 by Associate II
  • 3776 Views
  • 3 replies
  • 1 kudos

STM32L452xx Bootloader on UART4

I'm looking at AN2606, section 65.1 and it looks like UART 4 can NOT be used by the bootloader to load FW into the part. Can someone confirm that is true?

SKarl.19 by Associate II
  • 1029 Views
  • 1 replies
  • 0 kudos

I3C error in transmission/reception process - NUCLEO-H563ZI

I am using 2 Nucleo-H563ZI boards, one as controller and the other target, and referencing the knowledge base post "How to set up and run the I3C_Private_Command_IT controller and target example projects" yet I am getting an error. From what I can te...

Screenshot 2024-05-23 155815.png
JRM_02 by Associate II
  • 3102 Views
  • 4 replies
  • 0 kudos

Resolved! Núcleo-H755zi spi with NRF24L01

I'm trying to use Núcleo H7 spi 1 to send a message via radio with NRF24L01, the code using HAL worked perfectly on an Stm32F103 but when i try adapting it to the Núcleo it just don't work. Can somebody help me up? The SPI clock is 100MHz , the core ...

IMG-20240529-WA0005.jpg IMG-20240529-WA0004.jpg

STM32H7 SPI6 not working with DMA

Hello team, We have another challenge with STM32h725 controller, What I am trying to do and achieve is, Setup few external ADC over SPI bus with DMA. The ADC on SPIs other than SPI6 works perfectly. But the SPI6 is not with regular DMA but with BDMA....

Driver IHM16M1 burnt pin?

In the lab with a power supply (10V 0.5A) connected to the DC bus of the IHM16M1, the 3 phases of a DC motor, and some oscilloscope probes on the GPIOs of the STM32F302R8 I probably created a short (I don't know how, I deduce).I deduce this because n...

WhatsApp Image 2024-05-29 at 20.36.02.jpeg
luke514 by Senior
  • 1126 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H5 RTC count through power cycles

What is the expected RTC peripheral behavior through power cycles on VDD? We have a 3.3V system design with the STM32H562VGT6 right now.Setup:VDD = 3.3V from external supplyVBAT = 220mF supercap attachedRTC is enabled & counting, system is stableLSE ...

jreina by Associate III
  • 9352 Views
  • 11 replies
  • 10 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.