STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is there a list of MCU's with USB HOST controller?

I need a MCU with a USB host controller. It seems to be hit or miss as to which STM32 chips have this feature. I've tried the product selector on both this site and Digikey, but "host" is only ever listed in the datasheet, so this has proven fruitles...

Nucleo-l476rg interfacing with 74HC165B1

Hello Team,We are trying to configure Nucleo-l476rg with 74HC165B1 with SPI Parallel IN SERIAL OUT but unable to configure the board, Kindly help me with code with any other STM microcontroller in STMCUBE_IDE OR KEIL. Best Regards,Gagan Gowda G

ggowd.1 by Associate III
  • 1045 Views
  • 1 replies
  • 0 kudos

Stm32f103c8t6 Can't Start DMA ws2812b

 I want to drive a WS2812 LED strip using PWM and DMA. I've tried everything, but it's not working. I'm running at 72MHz, and I'm using htim2.Init.Prescaler = 0; and htim2.Init.Period = 90-1;. This is how my library works./** wsled.c** Created on: Ma...

nder by Associate
  • 1267 Views
  • 0 replies
  • 0 kudos

Multiple task run simultaneously || Multi-threading RTOS

Hello STM team,I'm working with STM32h745 project. in that interface 7 external ADC using SPI and I want to continuously read ADC data and send using serial usb. So now my function executed one by one sequential manner but Some ADC data loss. So I wa...

dplogiic by Associate III
  • 1032 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F411 SPI Flags Trigger Too Early

Hello all-Working with the SPI peripheral on the STM32F411VET6, we need to connect to a device that sadly requires the CS line to toggle with every byte sent.  Just about every example code runs along the logic of "write to the SPI data register and ...

Eqqman by Associate III
  • 2500 Views
  • 3 replies
  • 0 kudos

Resolved! Voltage admitted on an open drain output

Hello,I need to drive some power mosfets (STP55NF06) from open drain outputs.The gate and mcu output will be connected to a pull up resistor to 12VAre the TT and FT pin voltage limits applicable when used in open drain mode?If yes, I will amplify the...

xisco by Senior
  • 4503 Views
  • 7 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.