STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! UART receive buffers data instead of sending it to the code

Hi all, I'm trying to receive UART data from an xbee module, I've noticed the xbee is sending out the data correctly (using a logic analyzer) however the STM32L431KCU6 is not receiving this data properly and instead seems like the data is being buffe...

msingh08 by Associate III
  • 3064 Views
  • 5 replies
  • 1 kudos

Resolved! Can't configure DCMI peripherals

HelloI am starting a project with a STM32U585CIU6 and an OV7670 camera module. I want to use the DCMI interface to get the data, and I'm using the Introduction to DCMI to STM32 MCUs document as a reference.STM32U585 datasheet mentions the support to ...

LuizF_Ferro_0-1717415666926.png

STM32G474xx hrtim1

Hi, I have an inverter project designed with stm32g474xx and there is a "h-bridge" topology in the system.Can I create a uni-polar PWM to get three-level output while controlling this topology with hrtim1? Can hrtim1 generate two complementary PWM ou...

Kayhan by Associate
  • 1317 Views
  • 1 replies
  • 0 kudos

DAC trigger by HRTIM

Hi, I need to trigger DAC1 and DAC2 from HRTIM Timer A on a STM32G474. I have set the DAC Sync option inside the HRTIM Timer A settting to generate a DACTrigOut1 event that triggers my DAC1. But DAC has a separate Trigger event that also works for DA...

berait by Associate III
  • 1793 Views
  • 1 replies
  • 0 kudos

Bootloader on STM32H503RB via USB

We wish to bootload a STM32H503RB using USB. This works on the NUCLEO-H503RB, but after resetting the processor on our PCB with BOOT0 high windows reports "Device Descriptor Request failed".AN2606 states that CRS is enabled for the DFU to allow USB t...

CWedg.1 by Associate III
  • 5190 Views
  • 8 replies
  • 0 kudos

Unable to configure Ethernet as RMII

Hello Team, We are prepared our own board for Ethernet Configuration in STM32H745ZIT6 Board then configured peripherals what we need to use in ethernet after configuring ioc file while debug mode every time it will go error handler when it initialize...

ggowd.1 by Associate III
  • 5146 Views
  • 4 replies
  • 0 kudos

FMC timing calculation for NAND Flash

Hi Team,       I have gone through few documents and application notes for considering timing calculation for FMC to NAND, but still i did not get much understanding on this. Can anyone make me to understand how we need to calculate comspace, attribu...

SRAM read

Hi, Im referring F429 eval board fmc sram code. For Nucleo f439, I changed to bank 1 and bank addr=0x60000000 with R/W from e.g. and init from MX tool.The issue I see is on receive, the values are not the same (compared to TX) when buffer size>128 

GauravK by Senior
  • 2204 Views
  • 4 replies
  • 0 kudos

Resolved! Can VSSA voltage be slightly lower than VSS? (STM32H7, ADC)

I am wondering if VSSA voltage can be slightly lower than VSS? If so, what is the maximum allowed difference?The reason why I ask is because I would like to measure voltage slightly (0.2-0.3V) below the common ground attached to VSS. I looked in seve...

TDJ by Lead
  • 4326 Views
  • 7 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.