STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! power consumption vs. clock rate 32L4xx ?

hello all;i wondered if there are good guidelines for power consumption vs. clock, and, how low can the processor clock run? complex, i think, especiallly if one needs to run certain peripherals like ADC, or i2c... thanks!

Lohi by Associate III
  • 4073 Views
  • 7 replies
  • 4 kudos

Resolved! User timer interrupt for capture multiple time

Hi all,I'm working with STM32F4 discovery board, and I'd like to know if I can use one timer with interrupt to capture multiple time.For example I'd like to use TIM16, and be able to check 4 times : 150ms, 250ms, 500ms and 1000ms is it possible? Afte...

SBaro.11 by Associate III
  • 2246 Views
  • 3 replies
  • 0 kudos

STM32F446RET6 Nokia5110

I am using CMSIS for STM32F446RET6 (clock speed at 180 MHz) to drive Nokia5110 LCD Module via SPI1. But, this program doesn't work. When I test with STM32F103C8T6 (using CMSIS and Clock speed 72 MHz), Nokia5110 work well. Please help me. How to corre...

May by Associate
  • 1353 Views
  • 2 replies
  • 0 kudos

ADC Conversion time of STM32U5A5

Hello,i've implemented a routine to measure some ADC channels with the MCU STM32U5A5ZJ.After one measurement is finished (interrupt triggers after conversion) i start the conversion for the next channel.Settings:ADC conversion: Single conversion mode...

Shaheen by Associate II
  • 2356 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.