2024-06-14 5:11 AM
Hello,
i've implemented a routine to measure some ADC channels with the MCU STM32U5A5ZJ.
After one measurement is finished (interrupt triggers after conversion) i start the conversion for the next channel.
Settings:
ADC conversion: Single conversion mode, conversion length: 1 (i just want one conversion per channel)
ADC CLK: 1843200Hz
Sample Time: 5 Cycles
14 bit mode: 17 Cycles
TCONV = (5 + 17) ADC clock cycles = 22 ADC clock cycles = 11,9us
To check the whole conversion time i toggled a pin at the start and end of conversion and looked at the signal on the oscilloscope.
My result is 50us for the conversion time.
My question is:
Why is the conversion time so long? I expected 11,9us and i got 50us!
I appreciate any help.
LG
Shaheen
2024-06-14 5:48 AM - edited 2024-06-14 5:59 AM
Edit: Perhaps interrupt processing time in HAL. Reading and saving a timer clock is probably more accurate.
2024-06-14 5:54 AM - edited 2024-06-14 5:57 AM
The ADC CLK is derived from SYSCLK (SYSCLK = 1843200Hz = 1,84Mhz) I used the multiplexer to select the clk source for the ADC. So the CLK frequency should be fine.
2024-06-14 7:43 AM
Hi @Shaheen
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.