STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBPD with TCPP Package

Hi,I´m using the TCPP package (inside CubeMX). For my application I also need an ADC channel on the same ADC1 as used by TCPP to measure the Bus voltage. But it seems, that I don´t get any result in my application (configured as DMA). Investigating t...

AWack by Senior
  • 2137 Views
  • 3 replies
  • 1 kudos

STM32G030K8 eeprom emulation

Hi everybody,first an apologies for my poor English.I'm using STM32G030K8 in my project and I want to use eeprom emulation to save some parameters. I used the following code, however It didn't work. I spend a lot of time but I can find the problem. v...

Jimi by Associate II
  • 3436 Views
  • 6 replies
  • 1 kudos

STM32 Open Bootloader USB I/Fbug

In attempting to figure out how to stay in the bootloader loop while exchanging packets with the USB DFU tool I came across as what looks like an unintentionally undeleted line of code.Here is the code:static void OPENBL_USART_Go(void) { uint32_t a...

Resolved! Confusion on DMAMUX registers in RM0468

     Hallo everyone,Since some time I struggle to get DMA access working on a STM32H723. I was pointed out this MCU is a complicated beast, but I would at least expect sensible, coherent documentation for it.When I look at page 683, I see:on next pag...

Screenshot_Header_DMAMUX1_CxCR.png Screenshot_Header_DMAMUX2_CxCR.png Screenshot_Header_DMAMUX_RegisterMap.png Screenshot_RM0468_Bottom_P672.png
FredS by Senior
  • 4312 Views
  • 12 replies
  • 1 kudos

Resolved! H733: MCO output active without GPIO init

Heyho,so I was just checking the MCO1 output of my STM32H733ZGT6 and found some super jittery 64 MHz with full swing between 0V and 3.3V.Then checked my code and found that I had not set the RCC->CFGR and not even initialized the GPIO.When I actually...

LCE by Principal II
  • 5860 Views
  • 13 replies
  • 2 kudos

Resolved! STM32H5 - ADC DMA - Standard Request Example

HelloI am looking for an example to get the ADC regular sequence transferred by DMA to memory going.I use TIM15 to trigger the ADC regular sequence, which has four measurements, every 5 milliseconds. When I activate the EOS IRQ and toggle a GPIO I se...

IGärt.1 by Associate II
  • 4909 Views
  • 2 replies
  • 0 kudos

PWM sine gen two timers idea

Hi, req is generate sine wave and manage frequency precisely . My design require range 2Hz to 10Hz with for example step 0,002Hz.My idea is one PWM timer for sine with same table for exampel 10bit. Second linked timer for manage one sample time on PW...

MM..1 by Chief III
  • 1273 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.