STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ethernet Lwip Problem STM32H735

  /* add the network interface (IPv4/IPv6) with RTOS */ netif_add(&gnetif, &ipaddr, &netmask, &gw, NULL, &ethernetif_init, &tcpip_input); while(1){ /* Registers the default network interface */ netif_set_default(&gnetif); if (netif_is_link...

Kuttay by Associate III
  • 2420 Views
  • 3 replies
  • 1 kudos

Resolved! Baud rate of 4Mbps

Hello everybody,This is my first post hope i wll get the answer.I am building a spectrometer for which i am using a stm32f401re board and i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps so do i ...

000harsha by Associate II
  • 2736 Views
  • 3 replies
  • 1 kudos

Resolved! HSI vs HSE for CAN

Hi,On an Stm32f4 based board, we have the external crystal (8MHZ) mounted. The Firmware however uses HSI clock. Does the HSI drift have an impact on CAN communication with another device over a long period of time(say weeks)? Is it recommended to use...

krishr by Associate III
  • 2173 Views
  • 2 replies
  • 1 kudos

Resolved! CAN1 loopback does not work on STM32F427

Hello everyone,I have recently been trying to get the CAN1 bus working on the STM32F427. So far, however, it has not worked in either loopback or normal mode. For the normal mode I had a CANCaseXL Analyzer available. The problem, however, is that not...

Louis00 by Associate
  • 3076 Views
  • 3 replies
  • 3 kudos

BAUD RATE CALCULATION FOR USART IN STM32

PLEASE EXPLAIN WHY 104.167 IS CONVERTED TO 104.1875 AND HOW ITS ENCODED AS 0X683MY UNDERSTANDING FOR ENCODING IS 104 IS CONVERTED TO HEX AS MANTISSA PART AS DECIMAL TO HEX AND O.1875 IS CONVERTED SEPARATELY FOR FRACTION PART.IF I USE FCLK/BAUDRATE I....

0693W000004IhA6QAK.jpg
MMoba.1 by Associate
  • 22909 Views
  • 12 replies
  • 8 kudos

STM32U585 GPDMA with DCMI error

Hello,I am developing project where I need to do some image processing on BW image. All was great, but I started having problems with DMA (maybe I always had, don't recall)Idea is that I simply load data to internal SRAM with DMA, and when I get TC, ...

Linas L by Senior II
  • 1836 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.