2024-07-10 1:40 AM
Hello everybody,
This is my first post hope i wll get the answer.
I am building a spectrometer for which i am using a stm32f401re board and i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps so do i need to use 4Mbps baud rate to read that and if so how to achieve such higher baud rates.
Thank you.
Solved! Go to Solution.
2024-07-10 1:59 AM
From ds:
So whats the problem?
2024-07-10 1:51 AM
Hello and welcome to the community.
i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps
Not clear! Is it over a protocol communication? which one?
2024-07-10 1:55 AM
Yes it is over UART
2024-07-10 1:59 AM
From ds:
So whats the problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.