STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H563ZIT6 I3C master read buffer question

          Hello! I dont know where to find received data after HAL_I3C_Ctrl_Receive_IT progress.          I set I3C of my H563 as master and sent ENTDAA and master read , the slave answered both command. The interrupt of slave reflects that master re...

Xonier by Associate III
  • 3224 Views
  • 5 replies
  • 1 kudos

Resolved! stm32f722 SWD MEM-AP ports

I'm trying to see what's possible in terms of a bootloader in a custom application of an stm32f722. We have an external 2-megabyte flash chip on the QSPI bus, along with the internal 512-kilobyte flash.  I'd like to make the bootloader stored on inte...

bkadzban by Associate
  • 2805 Views
  • 2 replies
  • 0 kudos

UART transmitter issue in NUCLEO-F746ZG board

i am facing issue with uart transmission the data to the realterm software i didnot recieving the data to console i am attaching the code here #include "stm32f746xx.h" #include<stdint.h> #include "uart.h" int main(void) { uart4_tx_init(); RCC->AH...

Problem with external interrupt in PIN B2 stm32h753

Hello,I am working on a project with STM32H753XI mcu and with external interrupts. The problem is that I cannot take an interrupt to PIN PB2. Specifically:1.The Pin is configured as Rising Edge Interrupt (Also tested as falling edge and rising fallin...

SEfte.1 by Associate II
  • 1646 Views
  • 1 replies
  • 0 kudos

Unresolved Inclusion !!

Posted on December 28, 2016 at 07:18Hi,I think you might familiar with  this issue if you are proficient user of Eclipse +STM32.In my #include section of main.c file.Red error line indicates like :(,At the same time the system says to do indexer mar...

0690X00000605t6QAA.png 0690X00000605vaQAA.png

C16 burned in stm32 L010RB

While connecting the battery, the ground was inverted with the VCC and vice versa. As a result, this capacitor burned out. I need to know the function of this part and if I can continue to work normally after what happened. 

IMG_6646.jpeg
Minaihab by Associate III
  • 2745 Views
  • 4 replies
  • 0 kudos

Resolved! stm32f429 ethernet speed control

Hi,I want to make the system with stm32f4 series mcu. An important function of the system is to control the Ethernet speed.Is it possible to adjust the Ethernet speed with such detailed figures as 65Mbps, 38Mbps, and 300Kbps??If possible, how can I a...

inkong by Associate II
  • 4805 Views
  • 4 replies
  • 4 kudos

Resolved! STM32U5A9VJT6Q Power supply requirement

Hi I want to use the STM32U5A9VJ6Q_SMPS inbuilt chip in one of my projects. I plan to run the chip with 3.3V. Is it feasible to run at 3.3V for all pin functions?    

HPK by Associate
  • 1217 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.