STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750 Performance slows down after time

Hi!I have a problem with the canbus gateway project, I have a very good ring buffer that works without delays and transfers data between can1 and can2. All data copying is done through the main while loop where I check the buffers for can1 and can2 t...

sqwerize by Associate III
  • 10217 Views
  • 13 replies
  • 1 kudos

*STM32F030F4p6 Problem with GPIO_EXTI1 Pin*

Hello everyone,So I am trying to take Input from the sensor and then turn on the LED_1/Sound on and another senarove is that whne I prace the GPIO_EXTI1 turn on the another LED_2. but what is hapning is when senser is not givin Input even then LED_1/...

UART in full duplex missing bytes

Hello,I have an application where I transfer data to and from a PC with a FT232R and a UART. There is data beeing transfered back and foth constantly and asynchrone to another, so it is sending and receiveing at any random time and simultaneously. Se...

machinist by Associate III
  • 5073 Views
  • 8 replies
  • 2 kudos

Resolved! GDB-server openocd

Could not verify ST device! Please verify that the latest version of the GDB-server is used for the connection.Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD] Licensed under GNU GPL v2 ...

Kai_Satone_0-1715061177011.png

Resolved! STM32G0B1 EXTI DMA GPIO

Hello dear All,On STM32G0B1 I'm trying to capture PORTD[0-7] value with DMA on EXTI0 event (PD0 falling edge)(Read PORTD value in EXTI0 interrupt is too slow for this application -> PORTD change value before entering IRQHandler())I configure EXTI and...

MTE_MMO by Associate
  • 3712 Views
  • 3 replies
  • 0 kudos

stdlib bug - STM32F4 SPL (Standard Peripheral Library)

in stdlib version1.9.0, void I2S_Init(SPI_TypeDef* SPIx, I2S_InitTypeDef* I2S_InitStruct) { uint16_t tmpreg = 0, i2sdiv = 2, i2sodd = 0, packetlength = 1; uint32_t tmp = 0, i2sclk = 0; #ifndef I2S_EXTERNAL_CLOCK_VAL uint32_t pllm = 0, plln = 0,...

Ethan1_0-1720779658564.png
Ethan1 by Associate III
  • 3206 Views
  • 5 replies
  • 0 kudos

Application compiler error in STM32Cube_FW_F4

Hi there,I am using cubeMx to config the LwIP project which is based on STM32F429BI;I connect the MCU to the route and ping the MCU by PC successfully in DHCP or static IP mode.I can normally get the MCU IPv4 address in static IP mode but fail in DHC...

Junde by Senior III
  • 983 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.