2024-06-02 11:52 PM
Hello,
I am working on a project with STM32H753XI mcu and with external interrupts. The problem is that I cannot take an interrupt to PIN PB2.
Specifically:
1.The Pin is configured as Rising Edge Interrupt (Also tested as falling edge and rising falling edge).
2. The Interrupts in EXTI Line 2 are enabled with high priority. (I have tested to PI2 and I can take the interrupt).
3. The clock to port B is enabled.
4. I can read The Pin changes of the status (High-Low) from mcu. (I have tested this with the GPIO debbuging tool from keil and I see the changes and also with Polling the Pin).
The problem is that the mcu do not enter the callback function. I have tested with other pins and the mcu enters the callback function and all the system working as expected. Any Ideas?
Thanks In Advance,
2024-07-13 6:42 AM
Dear @SEfte.1 ,
can you share your code or any reduced SW able to reproduce it using PB2 for our community sanity check and help . It is a strange description / behavior .
Ciao
STOne-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.