Resolved! Cannot flash firmware through UART
Finally after a long struggle, I was able to get into the system memory by changing to CP2102 ttl wire. Now I have another problem. Any solution to fix this? The PCROP_PDP bit is unchecked also.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Finally after a long struggle, I was able to get into the system memory by changing to CP2102 ttl wire. Now I have another problem. Any solution to fix this? The PCROP_PDP bit is unchecked also.
Previously, I had a Raspberry Pi CM4 connected to an existing WebSockets server developed with Django Channels. The Raspberry Pi CM4 received data from an STM32F4 and forwarded it to the server. It also processed commands from the web server dashboar...
Hey everyone, new user here!In our project we are using:STM32F334R8T6STM32CubeIde Version: 1.14.1STM32CubeProgrammer release v2.17.0Debugger probe - Nucleo-F334R8 along with HAL implementation of handling communication using UART + DMA. Due to error ...
Hello, I have been working on the STM32G030K6T6 with DMX512 and TM1651 display for 8 months, and I am unable to find a solution to my problem.I am creating different patterns according to the DMX controller. One pattern involves the speed of blinking...
Hi!I'm a new STM32 user. I acquired a Nucleo-144 board today and noticed that there are no pins in CN11 & CN12. Just curious why.Thanks in advance.
We want to use HAL_SPI_Transmit to send data (master) in 8-bit units.However, even though we have set SPI_DATASIZE_8BIT, data is sent in 16 bits.Is there anything incorrect in the code below? uint8_t *spi_txdata;spi_txdata = (uint8_t *)malloc(2 * siz...
I am trying to change the system clock on my STM32F410RB using register programming. I have setup an SPI protocol to an external DAC IC which needs a minimum of 100ns (10MHz) clock period. The SPI allows for a maximum of 8MHz (fPCLK/2) at default clo...
Hello ,We are encountering an issue with the USART_DMA interrupt method on the STM32G070CBT6 microcontroller. The problem is that data is only received after performing a hardware reset. We expect the data to be received continuously without needing ...
I'm trying to get a simple UART hello world program to work. It just transmits a buffer once per second. I've enabled UART2, enabled the interrupt, and configured the baud rate, parity, and word length. But when I open minicom I don't see anything. I...
Hello,I am facing constant difficulties in connecting to my Nucleo H723ZG Boards.Almost every time I try to update the ST-Link via STMCube32IDE, the compilation stops half-way through the process and throws an error (see image)I have tried:swapping c...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.