STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

dynamic address broadcast not working for Nulceo-H563ZI

I just downloaded the "I3C_Controller_WakeUpFromStop" project for the Nucleo-H563ZI board using the example project import option. It compiled with no issues. Ran it with debugger and protocol analyzer on the I3C bus. When the subroutine "Handle_ENTD...

JRM_02 by Associate II
  • 1588 Views
  • 1 replies
  • 0 kudos

STM32H5 I3C SETGRPA

Hello !I am using the I3C interface between a STM32H563ZI and 2 LPS28 sensors. After a ENTDAA process I would like to send a SETGRPA but unfortunately it does not work. It seems the process fails during HAL_I3C_AddDescToFrame() due probably to a wron...

Capture d’écran 2024-07-17 à 16.35.13.png
Phil91 by Associate
  • 1448 Views
  • 1 replies
  • 0 kudos

Resolved! Clarifications regarding SPI transmission

I was working on a MP3 DECODER called VS1003. during reading the registers either i can send and receive data at SPI bus separately like  uint16_t result; uint8_t temp = 0; vs1003_control_mode_on(); delayMicroseconds(1); // tXCSS HAL_SPI_Transmi...

skuma.8 by Associate III
  • 1410 Views
  • 1 replies
  • 1 kudos

Resolved! I3C Dynamic Address

I'm using the I3C_Controller_ENTDAA_IT example to assign dynamic addresses to two BMA530 sensors, but I'm getting errors when running the code. Are there any modifications or additional steps I should consider to resolve this issue? I haven't made an...

Azad_0-1721655184264.png
Azad by Associate II
  • 1912 Views
  • 2 replies
  • 0 kudos

MCUBOOT bootloader upgrade OTA

Using following settings: IDE : VS Code (NRF connect plug-in) Programmer : Stm32Cube programmer Stlink Debugger  OS: Zephyr  MCU: Stm32u5 series   Modem: Sierra wireless I'm trying to upgrade MCUboot ( Zephyr's) bootloader using FOTA .I can upgrade a...

A Maq by Senior
  • 4895 Views
  • 3 replies
  • 0 kudos

Resolved! Signal Generator in AD9850

Hi Team,Can we interface AD9850 DDS Signal Generator Module with STM32F407G to generate sin wave and square wave, is there any procedure or links to interface between AD9850 with STM Microcontroller.Best RegardsGagan Gowda

ggowd.1 by Associate III
  • 2798 Views
  • 4 replies
  • 2 kudos

Resolved! STM32G4 and MCO pin

I am using STM32G431cbtx and enabling RCC_MCO. Since the STM32G4 supports two pins, PA8 and PG10, PA8 is being used for another function, and I am using PG10 for RCC_MCO. However, when measuring the voltage on pin PG10, it is always high. Can anyone ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.