2024-07-29 10:40 PM - last edited on 2024-12-10 7:19 AM by Andrew Neil
I was working on a MP3 DECODER called VS1003. during reading the registers either i can send and receive data at SPI bus separately like
uint16_t result;
uint8_t temp = 0;
vs1003_control_mode_on();
delayMicroseconds(1); // tXCSS
HAL_SPI_Transmit(&hspi2, &VS_READ_COMMAND, 1, HAL_MAX_DELAY); //command for read
HAL_SPI_Transmit(&hspi2, &_reg, 1, HAL_MAX_DELAY); //register
//READ DATA
HAL_SPI_Receive(&hspi2, &temp, 1, HAL_MAX_DELAY);
result = temp << 8;
temp = 0;
HAL_SPI_Receive(&hspi2, &temp, 1, HAL_MAX_DELAY);
result |= temp;
or i can do it using the function transmitReceive like
uint16_t result;
uint8_t temp = 0;
vs1003_control_mode_on();
delayMicroseconds(1); // tXCSS
uint8_t tx_data[] = { VS_READ_COMMAND, _reg };
uint8_t rx_data[2] = { 0, 0 };
HAL_SPI_TransmitReceive(&hspi2, tx_data, rx_data, 2, HAL_MAX_DELAY);
result = (rx_data[0] << | rx_data[1];
ISSUE i am facing is while transmitting the data using separate transmit and receive function it is working fine, but while using transmitrReceive function, i am unable to read any data.
Any suggestion would be highly appreceiable.
Solved! Go to Solution.
2024-07-30 1:02 AM
Well, SPI can be compared to a shift register: when one side is sent, the data in the buffer on the other side is shifted at the same time. So if your VS1003 does not yet contain the expected data in its own transmit register that you are currently requesting from the master with e.g. the command, TransmitReceive cannot produce anything meaningful.
Regards
/Peter
2024-07-30 1:02 AM
Well, SPI can be compared to a shift register: when one side is sent, the data in the buffer on the other side is shifted at the same time. So if your VS1003 does not yet contain the expected data in its own transmit register that you are currently requesting from the master with e.g. the command, TransmitReceive cannot produce anything meaningful.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.