STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Count number of pulses on TIM1 input on STM32G031

Hello,I have STM32G031 and I want to use PA8 pin (TIM1_CH1) to count pulses. My idea is to read number of counted pulses every 1 second and reset counter to 0. void TIM1_Init(void) { // Enable TIM1 clock RCC->APBENR2 |= RCC_APBENR2_TIM1EN; ...

StastnyPetr_0-1722952977228.png

STM32F4 LoRa E220-400T30S Communication

I got 2 STM32F446VET7 MCU board and I am trying to communicate each other with LoRa E220-400T30S.I cannot found any usefull libraries so I am trying to write one.I can communicate with modules from UART and setting configuration parameters.Both E22 m...

testbenchmark_0-1722767477601.png

STM32H563 Custom External Loader Issues

I am trying to build a custom external loader for W25Q64 SPI. I am using the OCTOSPI1 using the follow pins.PE11OCTOSPI1_NCSPF6OCTOSPI1_IO3PF7OCTOSPI1_IO2PF8OCTOSPI1_IO0PF9OCTOSPI1_IO1PF10OCTOSPI1_CLKI have followed the stm32-external-loader/Demo_Pro...

SWD lost when accessing NAND via FMC

Hello.  I am working with a STM32H563IIKX, connected to an external Macronix MX30LF2G28AD NAND Flash chip.  I have configured the FMC for NAND operation with what I think are correct parameters (this is completely new to me).I thought I'd try a very ...

Brian H by Senior
  • 1689 Views
  • 2 replies
  • 0 kudos

SMT32F767 HSI Clock Calibration

Hi,I am having uart baudrate problems while HSI clock as uart source clock. No problem with PCLK as source with the same uart. In Cube IDE (V1.16.0) and F7 software package (V.17.2), I get different values for HSI_CALIBRATION:Ide gets as 0x10 while r...

TKana1_0-1722926090116.png
TKana.1 by Associate III
  • 5035 Views
  • 12 replies
  • 3 kudos

STM32H745 power up issue

Hello,We are using the MCU STM32H745 in our current design.We have faced the issue of working MCU properly and below are the problem,Case 1 : At power ON, some time the MCU work properly and sometime does not work properly, when it is not work proper...

ABora.4 by Associate III
  • 9567 Views
  • 22 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.