STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H747I-Disco Examples combination issue

hello forumI'm trying to use two examples at once, I'm looking for a script to save an image on an SD card as Jpegthe examples are:BSPJPEG_EncodingUsingFs_DMAI'm trying to import the JPEG_Encoding example into the BSP one,While doing so, the compiler...

Resolved! STM32F446VET7 HardFault_Handler

HelloI design a PCB and I am using STM32F446VET7When I try to debug in competely clear project (created from STM32Cube IDE - Cube mx)I got the void HardFault_Handler(void) function after  SystemClock_Config();. With HSE or HSI dosent matter I got the...

testbenchmark_0-1723035868199.png

STM32 startup fails at HAL_RCC_ClockConfig

Hi, I have designed the custom board for STM32L073 series. Initially i have tested the code/firmware in Nucleo board of same part number, and we have designed the board keeping nucleo board schematic as reference. The code works fine in Nucleo board,...

Faizan75 by Associate II
  • 5929 Views
  • 8 replies
  • 3 kudos

Resolved! STM32H753ZIT6 ADC calibration DMA

Hi,I have setup the ADC in STM32H753ZIT6 to sample 4 channels with DMA in circular mode. This works as expected and I can check the values being updated in the "Live Expressions" tab.But there is an offset, which I can only get rid of, if I perform t...

tyassin_0-1723017604126.png tyassin_1-1723017640123.png
tyassin by Associate III
  • 1837 Views
  • 2 replies
  • 0 kudos

SPI communication between two STM3 boards

Hi All,Hope you are doing well.I am working on SPI communication between two STM32 boards (F7 as master and WB55 as slave), but I am encountering issues with reliable data transfer.The problem arises with the transfer of 2-byte data packets. Initiall...

Pluto7 by Associate II
  • 3300 Views
  • 4 replies
  • 0 kudos

Query on STM32G473CEU3

Hi,We are using STM32G473CEU3 in our designWe have a situation that when MCU is powered off, 3.3V appears on one of the IO pins from an external circuit with 2mA of sourcing. Will this damage the MCU or is it ok?

PY.1 by Associate II
  • 1348 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L071 and ADC channel 5 and 6 rank

Hello, I have configure ADC to use channel 5 and 6 but I am not understanding what I am doing wrong to get readings from the two channels. Here is my code:void adcConvertionFinish(ADC_HandleTypeDef* handle); static ADC_HandleTypeDef g_adc; static co...

teobarbs by Associate
  • 1386 Views
  • 1 replies
  • 1 kudos

Resolved! Issue in STM32H563ZI SAI_DMA Configuration

Hi, I am using PDM mems microphone to configure the STM32H563ZI SAI_A with GPDMA. I have attached the image of configuration details. After configuration I generate the code, But GPDMA initialization details not showing in the code. //  main.c  file ...

Srmssenthil_3-1721826245915.png Srmssenthil_4-1721826318911.png

Problem with PSRAM peripherals of STM32H735

Hello! I use the OSPI2 interface of the STM32H735IGK6 to connect to the ISS66WVO32M8DBLL and use indirect mode for memory reading and writing.1、The first step is to use cubemx to configure OSPI interface parameters as shown in the following figure:  ...

Lin_Yishan_0-1722994715086.png Lin_Yishan_1-1722994714722.png Lin_Yishan_2-1722994715331.png Lin_Yishan_3-1722994715328.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.