STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Core supply for STM32H573AII3Q

Hello, We are using STM32H573AII3Q in our application. It has in-built SMPS for core power supply. Just wanted to know can we disable this SMPS and use seperate external 1V LDO to power the core?

madhu1 by Associate II
  • 2232 Views
  • 2 replies
  • 0 kudos

Resolved! VREF Internal voltage reference G431 series

Hello,Can anyone suggest whether or not I need to connect external capacitors to the VREF+ pin if I plan to use VREF only for the onboard DAC?Could this be a hardware problem?STM32G431CBT6. The problem is that on the oscillogram I see oscillations wi...

Settings.png Oscillogram.png Pinout.png Capacitors.png
CrazyChel by Associate III
  • 2624 Views
  • 4 replies
  • 0 kudos

Setup PWM on TIM12 for trailing edge or leading edge

 Dear all,I have a custom pcb with a STM32H753 on it.There I'm already using the TIM12 function for generating a PWM output signal This is my init function - generated from CubeMX: void MX_TIM12_Init(void) { /* USER CODE BEGIN TIM12_Init 0 */ /...

img_temp_6429c917c5df00-74083290-87095399.png
julred by Associate II
  • 2167 Views
  • 4 replies
  • 0 kudos

Resolved! What is the correct connection for VCAP1 and VCAP2?

Hello,VCAP1 and VCAP2 are external capacitors for the core's voltage regulator.The data sheet for the STM32F479VI states that, "Stabilization for the main regulator is achieved by connecting an external capacitor CEXT to the VCAP1/VCAP2 pins."I inter...

Screenshot 2024-08-07 at 16.33.18.png exlabs_0-1723045268783.png Screenshot 2024-08-07 at 16.33.45.png
exlabs by Associate III
  • 3213 Views
  • 1 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.