STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Generate 10us single pulse triggered by software

Hello,I would like to generate a 10us wide single pulse using the hardware Timer 1 peripheral that can be triggered by software. Currently, I am setting a pin as GPIO output and manually setting the pin high and low. I was wondering if there was an o...

huzeifa by Associate
  • 1425 Views
  • 2 replies
  • 0 kudos

Stm32f411ceu6 usb dfu mode usb not recognized

I am a noob in electronics and i am trying to make a quadcopter drone.I found about stm32f411ceu6 inav firmware on internet github. I only used arduino before and this stm32f411ceu6 was my first one.I connected it with my laptop in dfu mode and used ...

Resolved! STM32U5x: USB ECM demo - how to setup host?

I am progressing on porting the CubeU5 project for STM32U575I-EV as Ux_Device_CDC_ECM to a NUCLEO-U575ZI-Q board: The USB enumeration seems to work: I hear the sound and I see also an USB "STM32 CDC ECM" device.BTW: very important to go with the righ...

USB_ECM_1.png USB_ECM_2.png
tjaekel by Lead
  • 16012 Views
  • 22 replies
  • 5 kudos

Resolved! STM32U585 IWDG Early Wakeup Interrupt and Stop modes

The manual I have for the STM32U585 describes the Independent Watchdog (IWDG) peripheral and says it has an Early Wake-Up Interrupt (EWI) feature.  The manual says "Wake-up from Stop with interrupt is supported only in Stop 0, Stop 1, and Stop 2 mode...

BDoon.1 by Associate III
  • 1989 Views
  • 1 replies
  • 0 kudos

HSE OSC configuration fails STM32H7S

I'm new to STM32. I made a custom board using STM32H7S3V8T6, but I think the HSE OSC configuration is failing. If I build main.c in (in Boot, not Appli), if (HAL_RCC_OscConfig(&RCC_OscInitStructure)!= HAL_OK) This part doesn't make HAL_OK, so this go...

111.png 222.png 333.png 스크린샷 2024-08-16 003050.png
cyn7 by Associate
  • 2005 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.