STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743 ADC3 Acquisition voltage accuracy

Now I want to use ADC3 to collect the voltage of single-ended signals. I used IN1 channel to collect the reference voltage source of 1.5V and the internal channel to collect the internal reference voltage source of the chip respectively. The test res...

hanqingze_1-1723211705777.png hanqingze_0-1723211675673.png
hanqingze by Associate III
  • 5619 Views
  • 8 replies
  • 0 kudos

STM32U0 1.8V and USB 3.3V

Hello! I am working with a STM32U073 on 1.8V and I want to use the USB feature. Indeed, the datasheet tells us that USB needs a separate power supply around 3V (4.1 Power supplies), but every time when I apply this voltage on VDDUSB pin, it goes to t...

Decebalus by Associate II
  • 3320 Views
  • 6 replies
  • 5 kudos

Resolved! BKIN Input to shutdown PWM for motor

Hi, i have configured BKIN pin to detect fault for my overcurrentSo for my motor driver if this pin sense BKIN input. How much time it be will taken by my microcontroller to sense and to act to shutdown my PWM gate signalsIs it hardware glued logic t...

sag_0-1723450589668.png
sag by Associate III
  • 3991 Views
  • 7 replies
  • 0 kudos

Resolved! NUCLEO-H723ZG Ethernet LWIP

hello alli am having stability issues with a sample code that uses ethernet with lwip and freertos.practically the operation is unstable, after a few resets it works but then hard faults appear:HardFault_Handler() at stm32h7xx_it.c:88 0x8000f88<signa...

AntoR by Associate III
  • 2934 Views
  • 3 replies
  • 1 kudos

USB device as MSC starting from cubeMx

Hello, I try to add MSC feature to my app. MCU is L452.To avoid side effects, I started a brand new app with cubeIDE/Mx.I activated USB_DEVICE feature.I declared the USB_DEVICE as mass storage class.I had a look to the MSC_standalone example from G0 ...

JulienD by Senior
  • 2155 Views
  • 2 replies
  • 1 kudos

only 1 byte RS485 received on STM32L051

Hi there I am using STM32L051 to talk to a RS485 transceiver and I am having problem with the receive part.System is as follow: laptop->FTDI USB converter-> Renesas transceiver -> STM32I want to update the single byte buffer when a character is detec...

STM32F4 Discovery Board

Posted on January 30, 2013 at 12:49Hello all, at the moment I have some issues with the voltages on the STM32F4 Discovery Board. The two diodes D1 and D3 (BAT60JFILM) causes a voltage drop around 0.32V, so that the 5V only delivers 4,68V and not 5V....

toeztuerk by Associate II
  • 4777 Views
  • 7 replies
  • 1 kudos

Resolved! STM32_Debugger_IC

I have a general question. I am using STM32F423 and STM32L407 Evaluation boards for practicing. So in both there boards they are using the debugger IC which is STM32F103CBT6.i.  Why are they using this IC and what exactly does this IC does in program...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.