2024-08-18 11:26 AM
I am having trouble configure the USB-C port for serial output. The board I got is a "BlackPill" and I have went to try some example code for USART2 and USART6, however, upon a reset, I still do not have a COM port appear. Any advice?
Solved! Go to Solution.
2024-08-18 3:34 PM
Where you expecting to see a com port when running a UART?
If you want to get something on USB connection, like a VCP, you have to run something that doing the handling on the USB bus: so use a serial to USB adapter, connected to the UART you want to use, or set in Cube the USB -> device -> virtual com Port, to let it include all the libraries and USB stack to do the action, that's needed for a USB VCP to work.
Read examples or here in forum how to use it then.
2024-08-18 3:34 PM
Where you expecting to see a com port when running a UART?
If you want to get something on USB connection, like a VCP, you have to run something that doing the handling on the USB bus: so use a serial to USB adapter, connected to the UART you want to use, or set in Cube the USB -> device -> virtual com Port, to let it include all the libraries and USB stack to do the action, that's needed for a USB VCP to work.
Read examples or here in forum how to use it then.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.