STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ask about the use of STM32U57XX MPU

Hi, the platform is STM32U57XQuestion:The variable is in the non secure area of SRAM.Why can't variable A in SRAM1 and variable B in SRAM2 assign values to each other after turning on MPU, otherwise it will trigger a hardware exception interrupt.Do y...

YunYang by Associate
  • 904 Views
  • 0 replies
  • 0 kudos

Update Firmware over USB Virtual Comm Port

Hello,I am using the STM32F373's virtual USB port successfully.  I can connect and send packets to the uC from a web browser.  I now want to allow the user to update the firmware from the web browser by uploading a file, instead of the traditional me...

LMorr.3 by Senior II
  • 9081 Views
  • 17 replies
  • 3 kudos

Free shipping ?

Dear Company,I bought eval board from e-shop. Order # ST36685. On Invoice is "Shipping & Handling (WS-STM32H73-EMEA-MAR25-2021) - $0.00" But today I receive invoice from ST - Invoice No: 60556478, and transfer fee is 350.44 USD. Total price for this...

SPrik by Associate II
  • 1566 Views
  • 2 replies
  • 0 kudos

Resolved! TIM3 periodElapsedCallback never called

In my code, after setting an on-board LED, the timer is started like this. __HAL_TIM_SET_COUNTER(&htim3, 0); while(HAL_TIM_Base_Start_IT(&htim3) != HAL_BUSY);In debugging mode, I saw that the CNT register was in fact incrementing, however in would al...

STM32F411 ADC DMA Output Issue

I have configured the ADC to use pins 1,2,3,4 for DMA transfer. I do get COM port output, however, I noticed that the outputted numbers aren't as they are supposed to be. The values for only 2 of the 4 pins change as they should. The other 2 do not.T...

dlaroche by Associate II
  • 1034 Views
  • 1 replies
  • 0 kudos

UART Communication

Hi I am trying to commuicate between two boards through UART.One board is nucleof4 and other board is a processor.Im sending a data from nucleo to other board(where data gets displayed) through HAL_UART_Transmit(&huart1,(uint8_t*)"Connect",sizeof("Co...

20240910_144134.jpg
harry123 by Senior II
  • 3239 Views
  • 6 replies
  • 5 kudos

Resolved! Ethernet MAC locks up when I flush the transmit FIFO

I have 2 boards, basically identical except one has PHY KSZ8091RNA and the other has KSZ8091RND.Both use the STM32F429NIH6.The only difference I can find in the two PHYs is that I need to set to set the REFCLOCK bit in KSZ8091RNA's PHYC2 register.  W...

STM32F407 Flash ERASE/WRITE error only after boot

Hello,      on an STM32F407 I am experiencing a Flash Erase/Write error. The odd things is that it happen only the first time after boot, the following times after the error I can write with no errors. But, if I erase and write in the Init phase, bef...

MRaff.1 by Associate III
  • 1906 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.