2024-09-11 10:05 AM
In my code, after setting an on-board LED, the timer is started like this.
__HAL_TIM_SET_COUNTER(&htim3, 0);
while(HAL_TIM_Base_Start_IT(&htim3) != HAL_BUSY);In debugging mode, I saw that the CNT register was in fact incrementing, however in would always rollover and would never trigger this callback function:
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(htim->Instance == TIM3)
{
while(HAL_TIM_Base_Stop_IT(htim) != HAL_BUSY);
HAL_GPIO_WritePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin, RESET);
}
}I saw on another forum post that someone suggested to put that code in stm32l0xx.c in the function TIM3_IRQHandler(). However when I did that, I found that the function was called instantly after HAL_TIM_Base_Start_IT(&htim3).
What is going on here? I opened a new project with the EXACT same settings for timer 3, and it worked perfectly. This project has become far too massive to move everything over to a new project without a lot of headache. I would prefer to find out how to solve this in the project I am currently working on. Here is the cubeMX configuration:
static void MX_TIM3_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim3.Instance = TIM3;
htim3.Init.Prescaler = 2047;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = 7811;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2024-09-12 6:55 AM
Some more information: I removed the function HAL_TIM_BASE_Stop_IT(), moved HAL_TIM_BASE_Start_IT() to the top of main(), and set a boolean value to indicate that the LED is set when I cleared the CNT register. in the interrupt callback, I check the timer instance and that boolean value to check whether the LED has been set. Now it's working flawlessly.
2024-09-11 10:41 AM
Do you have the TIM3 interrupt enabled in the NVIC? In CubeMX open the timer config window and click on the "NVIC Settings" tab.
2024-09-11 10:48 AM
Yes, those have been enabled since the start.
2024-09-11 11:57 AM
Here is some more information: I looked at the vector tables for both the original non-functioning program and the new functioning one. I found that TIM3_IRQHandler is mentioned in the non-functional project, but not the functional project.
2024-09-11 12:13 PM
attach your IOC file.
2024-09-11 12:20 PM
2024-09-11 4:50 PM
One thing i've noticed is that you're checking for HAL_BUSY when you call HAL_TIM_Base_Start_IT but the function only returns HAL_OK or HAL_ERROR. Not sure how you're getting past this or are you? You should be stuck here forever.
while(HAL_TIM_Base_Start_IT(&htim3) != HAL_BUSY);
You also check for HAL_BUSY in the callback. This will be a stuck forever loop as well
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(htim->Instance == TIM3)
{
while(HAL_TIM_Base_Stop_IT(htim) != HAL_BUSY);
HAL_GPIO_WritePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin, RESET);
}
}
Change HAL_BUSY to HAL_OK which should fix your issue.
2024-09-12 6:09 AM
I tried that method, and the interrupt worked once, but after that my B-L072Z-LRWAN1 board wouldn't receive LoRa data (this LED is an indicator for when data is received through LoRa). I switched the method to polling the CNT register and that worked with no issues. However, polling is not ideal. I would really like to know why this timer is malfunctioning like this in interrupt mode.
Another thing to consider, if the HAL_TIM_BASE_Start_IT() only returns HAL_ERROR or HAL_OK, it should always exit the while loop after 1 pass, since I am checking to make sure that the function does not return a value that it will never return. I still changed it to != HAL_OK though, just so it actually does something.
2024-09-12 6:55 AM
Some more information: I removed the function HAL_TIM_BASE_Stop_IT(), moved HAL_TIM_BASE_Start_IT() to the top of main(), and set a boolean value to indicate that the LED is set when I cleared the CNT register. in the interrupt callback, I check the timer instance and that boolean value to check whether the LED has been set. Now it's working flawlessly.
2024-09-12 8:03 AM
Another thing to consider, if the HAL_TIM_BASE_Start_IT() only returns HAL_ERROR or HAL_OK, it should always exit the while loop after 1 pass, since I am checking to make sure that the function does not return a value that it will never return. I still changed it to != HAL_OK though, just so it actually does something.
If you don't receive HAL_BUSY, then there is no way to exit the while loop.
Instead you've should have tested for the return status to be not HAL_OK
if(HAL_TIM_Base_Start_IT(&htim1) != HAL_OK)
{
// handle error
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.