STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H562 bootaloder

Hello,does STM32H562 have the system rom bootloader?I cannot find it AN2606, however its datasheet does mention the system bootloader.Thank you

tommz9 by Associate
  • 3114 Views
  • 5 replies
  • 1 kudos

volatile const

I need to declare a 'volatile const', meaning that the value is placed in FLASH and that it is re-read every time it is referenced (as the FLASH is written to elsewhere), but am finding it very difficult to accomplish this as the compiler either plac...

Ddu P by Associate III
  • 4884 Views
  • 6 replies
  • 0 kudos

Resolved! FreeRTOS in STM32U5

Hello,I was wondering if it is possible to use the FreeRTOS Middleware which is used on the STM32H7 and STM32F4 and which can be found at the following links ‘https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Middlewares/Third_Party/FreeR...

EnaitzO by Associate II
  • 1613 Views
  • 1 replies
  • 1 kudos

Resolved! Recommendation for stopping PWM signal

Looking for a recommendation for generating a discrete number of pulses from PWM, for the example below i setup timer 1 to generate PWM and timer 2 with input capture interrupt to count the pulses, I did this with both rising and falling edge and bot...

NoviceStm32_1-1726499192862.png DS1Z_QuickPrint2.png DS1Z_QuickPrint3.png DS1Z_QuickPrint4.png

Resolved! STM32F446RET6R TWO CAN PERIPHERALS

Hello!! I'm trying to use both CAN peripherals in an STM32F446RET6R on a custom PCB, but something is not going well enough. I've done the basic configuration using the STMCubeIDE platform (I'll add the code later, but first I want to know if someone...

Davaol19 by Associate III
  • 13500 Views
  • 30 replies
  • 2 kudos

Startup time of NUCLEO G431RB varies greatly

After troubleshooting this issue , i found, that i have a greatly varying startup time.I have this minimal code:int main(void) { /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); GPIO_InitTypeDef my_GPIO_InitStruct = {0}; // TEST PIN ...

Tobe by Senior III
  • 1730 Views
  • 2 replies
  • 0 kudos

Resolved! Unknown chip id! 0x421

Hello, so I am completely new to working with STM boards in general. I just got a brand new stm32f446re board, and I tried to upload some code to it through Linux. And I do mean brand new, I haven't uploaded or downloaded any code to it before this a...

Odega by Associate II
  • 12599 Views
  • 25 replies
  • 1 kudos

Resolved! netxduo mqtt application

Hallo,I have to question, all about netxduo.1. how to set the pool size of netxduo at the least value possible2. I need to use the mqtt client packet.  Is it necessary also to enable the arp protocol, icmp protocol, the TCP protocol, the udp protocol...

IVent.1 by Senior
  • 1372 Views
  • 1 replies
  • 0 kudos

two timer signals on one pin

Hi,Here is my problem, I need to output two different frequencies on one pin and I can't reconfigure the timer to new arr/psc values for a different frequency because these timers also output the frequency on other pins where the frequency/timer conf...

RLD by Associate II
  • 3332 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.