STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST-LINK error (DEV_TARGET_HELD_UNDER_RESET)

Hi I am working on a own prototype.The issue facing is NRST pin pulled low once powered on.Actually it should give me 2V.MCU used is STM32G030K8.and also on checking the PCB tracking its fine .When we checked by removing the MCU chip NRST is 2.0v .Wh...

meena by Associate III
  • 2098 Views
  • 1 replies
  • 0 kudos

Internal Loopback Test with QuadSPI

I am trying to test QuadSPI peripheral in the STM32H745BIT6 by carrying out an internal Loopback test. I am apparently not configuring its parameters correctly. Can anyone suggest what configurations I should do for QuadSPI and if there's anything wr...

Change timers output compare mode

Hello,I have a problem, I would like to change a timer output compare mode on my STM32G484xE microcontroller. I would like to switch between toggle and PWM mode 1. I do the whole thing with a small function for writing registers:void ProgRegister(uin...

Rafael1 by Associate
  • 1334 Views
  • 2 replies
  • 1 kudos

bootloader start application in ram, can't run task

hello:     I use NUCLEO-H7A3ZI-Q to implement a bootloader feature:the bootloader runs in 0x08000000 at flash, it'll copy the application stored in 0x08005000 to 0x24000000 in RAM, then jump to 0x24000000, if one LED turns on, indicates jumping to ap...

lbapplem by Associate II
  • 1096 Views
  • 1 replies
  • 0 kudos

Resolved! GPIO connections of OCTOSPI on external flash and ram

My MCU is the STM32H723. To save GPIO pins, I would like to use the following architecture:- Connect external HyperRAM and Flash to one OCTOSPI bus. - Use multiplexed mode to access OCTOSPIM_P1 and OCTOSPIM_P2.- Map external RAM and Flash to differen...

STM32G4 chaos in internal ref

Hi, i start design on G4 and am confused with internal ref in MX.1. Internal REF for ADC isnt real internal, but Vref2.Internal ref for comparators is 1/2 1/4 3/4 ... , but from what ?3. ADC stop working without VREF+ pin voltage, but comparator work...

MM..1 by Chief III
  • 1634 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.