STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Store values in STM32G0 internal flash

(was initially a reply to https://community.st.com/t5/stm32-mcus-products/store-values-in-internal-flash/m-p/666974 I am store variable in flash adders and after reset read but variable values is not store in flash adders.& using stm32g030f6p6 microc...

Resolved! Does HAL_UARTEx_ReceiveToIdle_IT deliver in chunks?

If I call HAL_UARTEx_ReceiveToIdle_IT to receive 512 bytes, will it wait till all 512 bytes are received before calling HAL_UARTEx_RxEventCallback or could it possibly call it several times, delivering fragments of the whole packet?I'm asking because...

KMill by Senior II
  • 2540 Views
  • 3 replies
  • 4 kudos

Resolved! STM32G0B1, CANFD issues

Hi guys! I have a custom board with 2x CAN FD transcievers (TCAN1057) and STM32G0B1 MCU. Everything works fine until i try to use hardware filters build into STM32. Whatever i do, filters don't pass any frame to RxFifo0/RxFifo1. The only way to recie...

ŁJura.1 by Associate II
  • 4008 Views
  • 6 replies
  • 0 kudos

Resolved! Printing values

I am using 16 sensors for my project and I need to print the sensor number and the corresponding signal strength for a ML model, but I am missing a lot of values. Is there an efficient way to do this?

slodh by Associate II
  • 2359 Views
  • 5 replies
  • 4 kudos

STM32G431KB ADC Wrong value

Hi everyone,I am using the ADC2 of the STM32G431KB to read a voltage value. I am actualy measuring 0.8V on the pin of the ADC with a multimeter, but while debuging, the conversion give me back 0.12V (~150 from the ADC, instead of ~1000). This is my c...

cppoisson by Associate II
  • 5278 Views
  • 13 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.