STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPUART receive data broken in STOP mode with LSE

Hello everyone:I'm working with board NUCLEO-U031R8, and need to wake up when LPUART receive data which using LSE with 32768Hz.MCU would send back the receive data which end with '\n', and it works fine in running mode, and a special command 'S' let ...

kein_2-1726454021135.png
kein by Associate III
  • 1339 Views
  • 1 replies
  • 0 kudos

NUCLEO-H7S3L8

I have a Nucelo-H7S3L8 board, but I accidentally burned the app into the boot, so I can't burn it again, what should I do?   err: 17:08:35 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using D...

loose by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L4A6 Exiting Stop Mode 1 using UART

Hi, Using references from 1) STML496 UART Wake up from Stop Example - https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Projects/NUCLEO-L496ZG/Examples/UART/UART_WakeUpFromStop/Src/main.c#L78 2) STM Getting started with PWR Guide - https:...

jlsw30_0-1726736464496.png
jlsw30 by Associate II
  • 2714 Views
  • 4 replies
  • 0 kudos

STM32H7 on simulink

I'm using matlab for debugging my stm32H7xx Nucleo board for blinking the LED. Everything is done but I'm having an issue while selecting the code generation system target file(Not getting the option of stm32.tlc instead getting ert.tlc) how to fix t...

VipulG by Associate
  • 2549 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L010K4TE x ST-Link-V2

I'm trying to use st-link v2 to program an STM32L010K4, but the stm32cube programmer doesn't identify this microcontroller (Error: No STM32 target found). The st-link is working, because I can program another STM32 without any problems. I appreciate ...

2D marking on the device show XXXX

Dear all , we bought STM32F429IIT6   DC 2337 from  agent , when we scan the 2D marking on the device show XXXXXXXXXXXXXXXX,   is it  normal ?  another question : we  found the PCN for the marking change  with  2D code  is from  2024-7-30 , but our de...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.