STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GCC/CodeSourcery toolchain on windows/linux ?

Posted on October 09, 2010 at 14:51has anyone succeeded in configuring a foss toolchain for stm32f100 (discovery board chip)? I have installed the latest codesourcery, and tried /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/flat.aspx?Roo...

izua by Associate II
  • 4454 Views
  • 9 replies
  • 0 kudos

question about interrups

Posted on October 18, 2010 at 15:28what will happen if during an interrupt routin another interrupt request will accure ? will the micro jump to the other or finish this routine and the jump to the other? thanks.

ezrab by Associate II
  • 1092 Views
  • 1 replies
  • 0 kudos

Interrupt Problem

Posted on October 17, 2010 at 11:32hi i am trying to activate the Tim2 Interrupt but for some reason it does not work here is the program i wrote: #include ''stm32F10x.h'' void setsystemclock(void); void TIM2_IRQHandler(void); int main(void) {     s...

ezrab by Associate II
  • 6876 Views
  • 18 replies
  • 0 kudos

Fast ADC

Posted on October 17, 2010 at 08:42hi. i have aquestion: if i want the measure sevrel channels in the fastest way what are my options and how? thanks.

ezrab by Associate II
  • 1442 Views
  • 3 replies
  • 0 kudos

Port I/O

Posted on October 16, 2010 at 21:34Hi, I'm new to the forum and the discovery board. Got it working with the test routines. Is it possible to switch a led, say LED5, connected to PC11, on and off using the routines in STM32_Discovery. If so how do I...

Bricked?

Posted on October 17, 2010 at 16:56Hello, I seem to have bricked my board. I have been experimenting with different compilers and linkerscripts, and probably something was messed up. None of the three IDEs will to establish contact with the board. T...

izua by Associate II
  • 1773 Views
  • 2 replies
  • 0 kudos

c++ code sample

Posted on October 15, 2010 at 13:30Hi, I'm going to try to write a few c++ sample projects. I'd like to use the ST demo board as target board. Is it possible to download some C++ project sample? Thanks Federico

ADC Conversion

Posted on October 12, 2010 at 13:22hi. i am trying to activate the adc module with the following program : __IO uint16_t ADCConvertedValue; int main(void) { int temp=0;     setsystemclock(); //set system clock to 24Mhz3     //rcc CONFIGURATION    RC...

ezrab by Associate II
  • 4000 Views
  • 12 replies
  • 0 kudos

Interrupt

Posted on October 14, 2010 at 16:17i understand that enabling the intrrupts is done while using the NVIC->ISER register but where can i find exactly how. what i meas is i could not find the description for each bit which bits i need to change in ord...

ezrab by Associate II
  • 887 Views
  • 1 replies
  • 0 kudos

Interrupt Problems

Posted on October 12, 2010 at 17:08hi i have aquestion about Interrupts: in all the example code that i saw i could never find where the program goes to in case of an Interrupt. here is one of the exmple code i have from st site which the button ac...

ezrab by Associate II
  • 904 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.