2010-10-15 4:30 AM
Hi, I'm going to try to write a few c++ sample projects.
I'd like to use the ST demo board as target board. Is it possible to download some C++ project sample? Thanks Federico2010-10-15 5:53 AM
I'm going to try to write a few c++ sample projects. I'd like to use the ST demo board as target board.
Is it possible to download some C++ project sample?
I don't think C++, and it's code size and runtime overhead is wholly appropriate for embedded micro controller work. For example C code, follow the link printed on the board and download the firmware library source which includes the library and sample/example projects. Would also suggest downloading the demo Keil or IAR tool chains.
http://www.st.com/mcu/contentid-133-110-STM32VLDISCOVERY.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.