Interleaved PWM
Posted on October 31, 2010 at 06:46hi. i have aquestion : is there any way to creater http://www.eetimes.com/electronics-news/4139692/Interleaved-PWM-controllers using stm32? thanks.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on October 31, 2010 at 06:46hi. i have aquestion : is there any way to creater http://www.eetimes.com/electronics-news/4139692/Interleaved-PWM-controllers using stm32? thanks.
Posted on October 27, 2010 at 15:27When using IAR Embedded Workbench with the STM32 Discovery, resetting the microcontroller with the interface does not reset the registers, nor memory.This is unexpected, and caused me to lose a lot of time. Is this...
Posted on October 25, 2010 at 14:28hi i am trying to activte TIM1 in complementary mode with dead time. but for some reason i get areverse dead time (both channels are at ''1'' instade of ''0'') why is that i could not find such an option in the man...
Posted on September 27, 2010 at 18:53Is it possible to export flash files from atollic TrueStudio using a separate tool rather than the stock ''flash converter - not included with the lite version'' ?
Posted on October 19, 2010 at 21:40Total noob at this, trying to (re-)build and launch the demo code on the Discovery board as a baseline.I'm running under Windows XP, downloaded and installed Atollic TrueSTUDIO lite.Discovery board is connected via...
Posted on October 06, 2010 at 15:35hi i was tring to activate USART3 On Port C PC10,PC11. i used this configuration : USART3->CR1 = 0x0C; //Receiver enable, Transmitter enable, USART disable USART3->CR2 = 0x0; USART3->BRR=156;//9600 at 24M...
Posted on October 19, 2010 at 15:14hi. i found out that it is possiable to use the flash as eeprom but the example i found was very long and complicated is there asimple way to do that? thanks.
Posted on October 20, 2010 at 11:29hi i saw that the slower watch dog i can make will reset after /* On Value line devices, Enable WWDG and set counter value to 127, WWDG timeout = ~1366 ×–s * 64 = 87.42 ms */ can i make it slower like 500msec? th...
Posted on October 18, 2010 at 20:21Hey There, after three days of succesfull playing with my stm32discovery i tried to attach a sd-card. After this i got an error while programming the new Firmware:C:/msys/1.0/build/tools/obj/gdb-7.1/gdb/regcache.c:...
Posted on October 12, 2010 at 17:45hi. i have ageneral question: what are the options to program the stm32 in mass production with minimum hardware? i would rather progrming would be after the unit was assambled. thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.