2010-10-12 8:08 AM
hi
i have aquestion about Interrupts: in all the example code that i saw i could never find where the program goes to in case of an Interrupt. here is one of the exmple code i have from st site which the button activate external Interrupt but where does the program goes in that case?? /** ****************************************************************************** * @file EXTI/main.c * @author MCD Application Team * @version V3.3.0 * @date 04/16/2010 * @brief Main program body ****************************************************************************** * @copy * * THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS * WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE * TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY * DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING * FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE * CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS. * * <h2><center>© COPYRIGHT 2010 STMicroelectronics</center></h2> */ /* Includes ------------------------------------------------------------------*/ #include ''stm32f10x.h'' #include ''stm32_eval.h'' /** @addtogroup STM32F10x_StdPeriph_Examples * @{ */ /** @addtogroup EXTI_Example * @{ */ /* Private typedef -----------------------------------------------------------*/ /* Private define ------------------------------------------------------------*/ /* Private macro -------------------------------------------------------------*/ /* Private variables ---------------------------------------------------------*/ /* Private function prototypes -----------------------------------------------*/ /* Private functions ---------------------------------------------------------*/ /** * @brief Main program. * @param None * @retval None */ int main(void) { /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f10x_xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f10x.c file */ /* Initialize LED1 and Key Button mounted on STM3210X-EVAL board */ STM_EVAL_LEDInit(LED1); STM_EVAL_PBInit(BUTTON_KEY, BUTTON_MODE_EXTI); /* Generate software interrupt: simulate a falling edge applied on Key Button EXTI line */ EXTI_GenerateSWInterrupt(KEY_BUTTON_EXTI_LINE); while (1) { } } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { } } #endif /** * @} */ /** * @} */ /******************* (C) COPYRIGHT 2010 STMicroelectronics *****END OF FILE****/ thanks...2010-10-12 9:16 AM
i have aquestion about Interrupts:
in all the example code that i saw i could never find where the program goes to in case of an Interrupt.
here is one of the exmple code i have from st site which the button activate external Interrupt but where does the program goes in that case??
Typically the interrupt routines are in the file stm32f10x_it.c within the project. /** * @brief This function handles External line0 interrupt request. * @param None * @retval None */ void EXTI0_IRQHandler(void) { if(EXTI_GetITStatus(USER_BUTTON_EXTI_LINE) != RESET) { /* Toggle LED3 */ STM32vldiscovery_LEDToggle(LED3); /* Clear the User Button EXTI line pending bit */ EXTI_ClearITPendingBit(USER_BUTTON_EXTI_LINE); } }
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.