STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32VLDiscovery with KEIL µVision4 IDE crash on load/debug

Posted on April 02, 2011 at 06:26Hey everyone!This is my first time here and a complete novice with this microprocessor.We are using it (STM32VLDiscovery) for our Senior Design Project in Electrical/Computer Engineering. We just switched from anothe...

aj1 by Associate II
  • 2487 Views
  • 5 replies
  • 0 kudos

Error Message: No STLink detected as normal user

Posted on March 04, 2011 at 14:42 Hallo, I have installed MDK-ARM 4.14 on Win XP and using a STM32- Discovery board. My problem is the Flash download of my project: When I run download as ''normal'' user I get the ErrorMessage (PopUp) which says: ''...

dom_4567 by Associate
  • 1877 Views
  • 3 replies
  • 0 kudos

GPIO's On external target not working

Posted on March 28, 2011 at 18:38Hello everyone.I'm trying to get the gpio's working on an external target (st32f103zd).I'm using the Atollic Truestudio lite STM32 discovery ide.The code i'm using works fine on the ''internal target'', the mcu on th...

timistof by Associate III
  • 1845 Views
  • 5 replies
  • 0 kudos

stm32vl discovery layout

Posted on February 28, 2011 at 01:03Hi, I want to use the board on top of a ''motherboad'', so I need STM32 VL Discovery layout (or just P1, P2 and P3 layout dimensions), where can I find it? thanks in advance.

gevides by Associate II
  • 2806 Views
  • 7 replies
  • 0 kudos

Flash - writing help

Posted on March 25, 2011 at 19:58I am new to all of this. I got the board from a classmate.I am trying to store accelerometer data in the flash during an experiment. Then, retrieve it when I plug the board into the computer via the USB. I am struggl...

Upgrading the Discovery with STM32F103

Posted on March 14, 2011 at 16:20I've got STM32F103RET6 chip, 72 MHz, 512K flash and 64K RAM. The chip seems to be pin-to-pin compatible with the STM32F100RBT6. What if I replace the original chip with this more powerful one? Has anyone ever tried t...

kuchura by Associate
  • 1875 Views
  • 3 replies
  • 0 kudos

Interfacing the STP1612PW05 16-channel LED Driver

Posted on December 14, 2010 at 19:52Can anyone point me to a more detailed interfacing document than what is provided in the datasheet for this chip? Specifically, I need to understand (preferably by real-world program examples) how to program the S...

DAC control register

Posted on March 11, 2011 at 10:15hi, i use a STM 32 discovery , and i would like to use the DAC without the library. i make my driver , a pointer initialised on the address 0x4000 7400, and a function for write the value 0x0003 0003 in the control r...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.