2011-04-01 10:17 AM
All:
I'm trying to get my STM32Discovery board to talk to a NewHaven LCD display/controller C0220BIZ-FS(RGB)-FBW-3VM via I2C and have encountered some problems. I managed to piece together the following code from various examples found online but I don't know if I have the initialization strings right. Put simply, I don't know what I'm doing and the code doesn't work. I double checked my wiring with the NewHaven support folks and I believe I have that built correctly. Howver, without a logic analyzer, I'm not sure if the board is even outputting I2C. Q: Would one of you folks mind taking a look over this program to see if I've gotten the I2C interface initialized correctly or not? It would be nice to have a ''known'' good I2C example that I could readily adapt to my needs. Thanks in advance for your replies. Regards, -g/*****************************************************************************
* @file main.c * @author Gunn * @version V3.1.0 * @date 03/21/2011 * @brief Test I2C interface to LCD ****************************************************************************** * *//* Includes ------------------------------------------------------------------*/
&sharpinclude ''stm32f10x.h'' &sharpinclude ''STM32vldiscovery.h'' &sharpinclude ''stm32f10x_i2c.h''/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*///I2C LCD Defines
&sharpdefine LCDSlave 0x78 &sharpdefine LCDComSend 0x00 &sharpdefine LCDDataSend 0x40/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/ GPIO_InitTypeDef GPIO_InitStructureOutput; // Structure for Output Definitions GPIO_InitTypeDef GPIO_InitStructureI2C; // Structure for I2C DefinitionsI2C_InitTypeDef I2C_InitStructure; // Structure for I2C
/* Private function prototypes -----------------------------------------------*/
void Delay(__IO uint32_t nCount); void LCD_Init(void); void LCD_Show(unsigned char *text); void LCD_NextLine(void); /* Private functions ---------------------------------------------------------*/int main(void) {
/* Enable Clocks */ RCC_APB2PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); // Enable I2C Clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); // Enable GPIOC Clock/* Init Outputs */
GPIO_InitStructureOutput.GPIO_Pin = LED3_PIN | LED4_PIN; GPIO_InitStructureOutput.GPIO_Mode = GPIO_Mode_Out_PP; // Push Pull aka Correct Mode to output LED on wire GPIO_InitStructureOutput.GPIO_Speed = GPIO_Speed_50MHz; // Correct Speed to output LED on output wire GPIO_Init(GPIOC, &GPIO_InitStructureOutput); // Send Struct// I2C CONFIGURATION --------------------------------------------------------/
// Configure all GPIOB in open drain AF mode (for different I2C levels) GPIO_InitStructureI2C.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructureI2C.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructureI2C.GPIO_Mode = GPIO_Mode_AF_OD; // Initialise the GPIOB Peripheral GPIO_Init(GPIOB, &GPIO_InitStructureI2C); // Configure the GPIO ports as alternate functions (PB6,7) -- already initialized above? // GPIO_PinRemapConfig(GPIO_Remap_I2C1, ENABLE);// I2C CONFIGURATION ---------------------------------------------------------/
// Declare an I2C_InitTypeDef structure, with I2C_InitStructure variable
// Fill the variable with allowed values of member structure I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; //only effects fast mode I2C_InitStructure.I2C_OwnAddress1 = 0x03A2; // Alt example 0xA0 I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = 100000; // Alt example 400000 // Initialise the I2C1 peripheral I2C_StructInit(&I2C_InitStructure); // Enable I2C1 peripheral (alt example says do this first before init struct) I2C_Cmd(I2C1, ENABLE); */ //Init Onboard LEDs output STM32vldiscovery_LEDInit(LED3); STM32vldiscovery_LEDInit(LED4); STM32vldiscovery_LEDOff(LED3); // turn LED off STM32vldiscovery_LEDOff(LED4); // turn LED off // LCD_Init(); while (1){ STM32vldiscovery_LEDOff(LED4); LCD_Show(''Hello World!''); Delay(0xAFFFF); STM32vldiscovery_LEDOn(LED4); // Blink LED to tell me its in the loop}
}/**
* @brief Inserts a delay time. * @param nCount: specifies the delay time length. * @retval None */ void Delay(__IO uint32_t nCount) { for(; nCount != 0; nCount--); }/**************************************************** n
* Initialization For ST7036i * *****************************************************/void LCD_Init(void) {
I2C_GenerateSTART(I2C1,ENABLE); // Alt example says no need to ever disable I2C_SendData(I2C1,LCDSlave);//LCDSlave=0x78 I2C_SendData(I2C1,LCDComSend);//LCDComSend = 0x00 I2C_SendData(I2C1,0x38); Delay(0xAFFFF); // I think this is 50ms I2C_SendData(I2C1,0x39); Delay(0xAFFFF); // I think this is 50ms I2C_SendData(I2C1,0x14); I2C_SendData(I2C1,0x78); I2C_SendData(I2C1,0x5E); I2C_SendData(I2C1,0x6D); I2C_SendData(I2C1,0x0C); I2C_SendData(I2C1,0x01); I2C_SendData(I2C1,0x06); Delay(0xAFFFF); // I think this is 50ms I2C_GenerateSTOP(I2C1,ENABLE); // Alt example says no need to ever disable }/****************************************************
* Send string of ASCII data to LCD * *****************************************************/ void LCD_Show(unsigned char *text) { int n; //int d=0x00; I2C_GenerateSTART(I2C1,ENABLE); // Alt example says no need to ever disable I2C_SendData(I2C1,LCDSlave); //LCDSlave=0x78 I2C_SendData(I2C1,LCDDataSend);//Datasend=0x40 for(n=0;n<20;n++){ I2C_SendData(I2C1,*text); ++text; } I2C_GenerateSTOP(I2C1,ENABLE); // Alt example says no need to ever disable } /***************************************************** * Send a NextLine to LCD * *****************************************************/ void LCD_NextLine(void) { I2C_GenerateSTART(I2C1,ENABLE); // Alt example says no need to ever disable I2C_SendData(I2C1,LCDSlave); //LCDSlave=0x78 I2C_SendData(I2C1,LCDComSend);//LCDComSend = 0x00 I2C_SendData(I2C1,0xC0); I2C_GenerateSTOP(I2C1,ENABLE); // Alt example says no need to ever disable }/*****************************************************/
#i2c-stm32vl-discovery-lcd2011-04-01 11:41 AM
/* Enable Clocks */
RCC_APB2PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); // Enable I2C Clock Should be RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); // Enable I2C Clock You don't need the ReMap, the I2C1 is the default AF function for PB6/7 You'll need to enable the GPIO B clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); // Enable GPIOB ClockWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.