2011-03-04 5:42 AM
2011-03-04 10:11 AM
Can any one help?
Try Keil technical support. Try your own IT people. Perhaps there is a security or policy setting on your XP system that precludes the use of external USB devices.2011-03-29 11:14 PM
Hello,
I have the same Problem as stated below: Normal-User -> No Flashing, Administrator -> it seem to work fine. The issue is the same (just with different error messages) in Keil, Atollic TrueStudio Lite and IAR KickStart (6.10). Has anybody an Idea which helps in ether of the above systems? The SDW is set correctly. Could there be an Problem with the Firewall or Avira, because one time I tried Atollic as ''Admin''t, a WindowsXP-Firewall-Window popped up and stated that ''gdb-server'' has been blocked and asked how to deal this issue in future ?2011-03-30 1:41 AM
It could be a number of things including driver signing, or other policy settings either for security or virus scanning.
Are you on a domain? Is there a reason you can't be an admin, power user or have a user with administrative rights, on your own machine? I don't believe XP or Vista come broken this way out of the box. If it is a company policy, get the clowns in IT to come fix it. If you are opening sockets you'll need to have the application or ports in the firewall's exception list. http://support.microsoft.com/default.aspx?scid=kb;en-us;555324 http://www.keil.com/support/docs/2937.htm In Vista there are things like UAC to watch out for. Cross posted here http://www.keil.com/forum/17985/We’re moving the ST Community to a new platform to give you a better and more reliable community experience.