STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with STM32F105VC using 8MHz crystal

Posted on July 15, 2011 at 19:58Hi,I have spent the better part of the day trying to get code that run perfectly on an STM32F107VC using a 25MHz crystal to run on an STM32F105VC with an 8 MHz crystal. We are using v3.5.0 of the library from ST.Chang...

STM32 GPIO Configuration utility????

Posted on August 04, 2011 at 12:41Hello there...My aim is, I need to be able to configure ports of stm32. Is there an utility/software in order to configure GPIO of it?Any help, feedback will be so helpful!..

ST-LINK V2

Posted on July 29, 2011 at 23:24I would like to know if the ST-LINK V2 allow to set a breakpoint while de code is running. I'm using EWARM 6.21.

Asantos by Senior
  • 1020 Views
  • 2 replies
  • 0 kudos

stack use monitor

Posted on August 03, 2011 at 15:06I'd like to add stack usage monitoring to my application. I can't afford the overhead of stack checking on every function call, so I was considering adding a routine that runs periodically to monitor the stack high-...

RTCK,DBGREQ,DBGACK needs mandatory pulldown to ground?

Posted on July 30, 2011 at 12:46Hi, I am using a STM32F100CB part on my target. I have not pulled RTCK, DBGRQ and DBGACK down with a 10K as recommended by the App note AN2586. Presently I am not able to get Ulink2 to communicate with my target. I ge...

gopi by Associate
  • 1488 Views
  • 2 replies
  • 0 kudos

Hard fault with no obvious reason why

Posted on August 03, 2011 at 18:50I'm running into a hard fault situation and I'm not sure why this is happening.From what I'm seeing in the fault status registers I'm getting...Usage fault status: INVSTATE is setHard fault status : FORCED is setDeb...

shotaro by Associate II
  • 1791 Views
  • 2 replies
  • 0 kudos

DEV_TARGET_CMD_ERR on breakpoints (Rowley Crossworks)

Posted on May 30, 2011 at 01:57I've just gotten some STM32VLDiscovery boards and am attempting to program them via Rowley Crossworks.  I've got the STLink connection working and can download and run programs and view registers, etc.  But if I try to...

kk6gm by Associate II
  • 960 Views
  • 2 replies
  • 0 kudos

Programming Ethernet on STM32-P107

Posted on July 21, 2011 at 10:15 Hi guys, Does anyone know how to configure the RMII mode which include the signals: TXD, TX_EN, RXD, CRS_DV, MDC, MDIO, REF_CLK. an explication, or an example configuration would be very helpful, Thanks in...

brouzi by Associate II
  • 1371 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.