2011-07-15 10:58 AM
Hi,
I have spent the better part of the day trying to get code that run perfectly on an STM32F107VC using a 25MHz crystal to run on an STM32F105VC with an 8 MHz crystal. We are using v3.5.0 of the library from ST.
Changing the HSE_VALUE either directly in the header file or via a definition get the UARTs (or at least the one I have tested) to run at the correct speed. The problem is the timers that run a factor 25/8 slow. The value of the SystemCoreClock variable is set to 72MHz by SystemInit(), as expected.
Any help available?
TIA
/Janne
#hse_value-external-clock-connectivity-line #utsl2011-07-15 11:50 AM
Probably because system_stm32f10x.c has stupid code like this for the ''STM32F10X_CL'' which presumes HSE = 25 MHz, correct ALL of these and it'll work fine.
/* PLL2 configuration: PLL2CLK = (HSE / 5) * 8 = 40 MHz */ /* PREDIV1 configuration: PREDIV1CLK = PLL2 / 10 = 4 MHz */ RCC->CFGR2 &= (uint32_t)~(RCC_CFGR2_PREDIV2 | RCC_CFGR2_PLL2MUL | RCC_CFGR2_PREDIV1 | RCC_CFGR2_PREDIV1SRC); RCC->CFGR2 |= (uint32_t)(RCC_CFGR2_PREDIV2_DIV5 | RCC_CFGR2_PLL2MUL8 | RCC_CFGR2_PREDIV1SRC_PLL2 | RCC_CFGR2_PREDIV1_DIV10);2011-07-15 11:51 AM
I am guessing that you are connecting the HSE directly to SYSCLK instead of passing it through the PLLCLK where the 8 MHz is multiplied to get the SYSCLK frequency. Note that 25 is not an integer multiple of 8, so you will have to readjust the timers anyway.
The USART frequencies are automatically adjusted for SYSCLK frequency, which is why everything is wonderful there. If the above is not the answer, post your code so that we don't have to guess anymore. Cheers, Hal2011-07-15 12:01 PM
The system is almost certainly NOT running at 72 MHz. The USART's work because the library works the math backward on actual the PLL setting and the HSE_Value, no doubt computing that your system is, in fact, running at 23.04 MHz
Try printing the value out RCC_ClocksTypeDef RCC_ClocksStatus; RCC_GetClocksFreq(&RCC_ClocksStatus); printf(''%d %d %d\n'', RCC_ClocksStatus.SYSCLK_Frequency, RCC_ClocksStatus.PCLK1_Frequency, RCC_ClocksStatus.PCLK2_Frequency);2011-07-15 1:20 PM
Thank you both for your replies. I guess this is what happens when you try to be ''modern'' and reuse canned code. I will try to get it up and running tomorrow.
I completely agree that the library is full of stupid code. And what's the point of having a variable with the system frequency when you can't trust it? And when it's not used in other library code.
Thanks again, I will report back tomorrow.
/Janne
2011-07-16 12:58 AM
Problem solved! Thank you for your help!
If anyone is interested I have an ugly fix.
/Janne
2011-08-05 4:46 PM
Most of the evaluation boards for the Connectivity Line use 25 MHz crystals. Does anybody know why? Does that come out to better frequencies for USB OTG or Ethernet or something? It sure makes you do some funny math with PPL2 (/5 x8 /5) just to get back to 8 MHz!
Otherwise, we'd rather standardize on 8 MHz crystals for both CL and XL parts.2011-08-05 5:01 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.