2011-07-29 2:24 PM
I would like to know if the ST-LINK V2 allow to set a breakpoint while de code is running.
I'm using EWARM 6.21.2011-08-04 4:19 AM
Yes ST-Link allows to set break points while STM32 based applications running.
2011-08-05 5:51 AM
Do you mean ST-LINK V2? Because I tested ST-LINK with EWARM and it doesn't allow that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.