STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CPAL, DMA and IT priority.

Posted on August 07, 2011 at 00:17Hello,I work on a product with master I2C rx and tx, MCU is STM32F295RG.I started with home made I2C functions for reading and writing using pattern ''send something and brute force while until it's finished'', but ...

root by Associate II
  • 1579 Views
  • 4 replies
  • 0 kudos

CAN status pending

Posted on August 08, 2011 at 11:55I wanted to run the CAN Interface of a  STM32F105RB with the examplefile of ST (Can Network). The function  CAN_TransmitStatus( CANx, 0x0) tells me that the status of transmission is pending. Do you have any idea's ...

mic by Associate II
  • 3209 Views
  • 4 replies
  • 0 kudos

Keil and binary file

Posted on August 08, 2011 at 10:37hello everybody,Do you know how to load a binary file into an STM32 Dicovery using Keil (and JTAG), without having the source code? I mean, I do not have a project I can compile, create a binary file and then downlo...

edxxgardo by Associate II
  • 1593 Views
  • 2 replies
  • 0 kudos

Problem with STM32F105 USB

Posted on August 03, 2011 at 11:48I have a big problem with configuration of USB on STM32f105VBT6. I'm trying to run HID example from ST USB Library but it doesn't respond at all. Message that I get is USB Device not recognized. I've tried to run th...

IAR workbench + ST-Link/V2 Reset problem

Posted on August 08, 2011 at 12:25Hi All, Chip: STM32F100C4 Custom board Need some help. I download the program via from IAR embedded workbench flash loader using ST-Link/V2. Every thing is ok. But i have to manually reset the pin no.7 to get it wor...

jai2 by Associate
  • 2735 Views
  • 3 replies
  • 0 kudos

CAN transmit status pending (STM32F105RB)

Posted on August 08, 2011 at 11:54I wanted to run the CAN Interface of a  STM32F105RB with the examplefile of ST (Can Network). The function  CAN_TransmitStatus( CANx, 0x0) tells me that the status of transmission is pending. Do you have any idea's ...

mic by Associate II
  • 911 Views
  • 0 replies
  • 0 kudos

Can PA0 have a dual use for ouput and WKUP?

Posted on August 06, 2011 at 20:47After WKUP I want configure PA0 for output, then at some point configure for WKUP and go into STANDBY deep sleep mode.  It appears that once the EWUP bit is set in RCC_CSR a) the EWUP bit cannot be reset unless ther...

C Plus Plus

Posted on August 06, 2011 at 09:11&sharpifdef __cplusplusextern ''C'' {&sharpendifI've seen the above in all the library header files , but what does it mean? #mix-c-and-c++

greg_t by Associate II
  • 1609 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.