STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cant connect to stm32 discovery

Posted on October 01, 2011 at 00:11I have a problem with stm32 discovery. I am using IAR 6.21.3 and I constantly get the following error:Fatal error: Faild to read CPUID from Cortex deviceSession aborted!ST-Link Utility is also giving me an error:No...

shinobi by Associate
  • 1008 Views
  • 2 replies
  • 0 kudos

STM32F100 RXNE Problem

Posted on October 01, 2011 at 18:45Hi everyone! I have some problem with USART interrupt while receiving. RXNE bit clearing automatically by entering the interrupt without any actions, therefore software cannot detect character received event. I use...

modus by Associate
  • 729 Views
  • 0 replies
  • 0 kudos

how to access a slave I2C device ID with STM32 master I2C?

Posted on October 01, 2011 at 08:04Hi all,I'm using discovery kit. Does anyone know if STM32 I2C master supports 24-bit device ID reading from an I2C slave? I have a slave compliant to I2C rev 03 standard and I need to read it's device ID with my st...

brazov22 by Associate II
  • 809 Views
  • 0 replies
  • 0 kudos

STM32F205 TIM2 Capture

Posted on September 27, 2011 at 12:04Is it possible to use the timer clock prescaler in input capture mode? I used some different values but that doesn't seem to make a difference, the value in TIM2->CCR3 is the same every time. 

cm600 by Associate II
  • 1812 Views
  • 5 replies
  • 0 kudos

Using 5 UARTs at the same time

Posted on September 30, 2011 at 00:08I am using an STM32F103ZE but could switch to a different model. I need to have all five UARTs running at the same time to receive data from different peripherals.  Originally I was thinking of having 5 ISRs to h...

jprinster by Associate II
  • 2147 Views
  • 4 replies
  • 0 kudos

Battery measurement.

Posted on September 27, 2011 at 13:26Good morning all, First of all, my project:Measure the voltage, current en temperature with an ADC from the STM32 Value Line Discovery. Sending this data to the computer with UART (RS232). The load on the batter...

Is PB5 really not 5V tolerant?

Posted on September 29, 2011 at 18:35The data sheet I have says it isn't, and yet it's not an ADC input as all the other non 5V tolerant pins seem to be.  Of course I'll believe the datasheet if there's no positive information that it's wrong, but i...

kk6gm by Associate II
  • 2399 Views
  • 4 replies
  • 0 kudos

STM32F103 with LIS331DLH (SPI)

Posted on September 29, 2011 at 13:25Hi, is there any samplecode that shows how the LIS331DLH Mems Accelerometer works with SPI Communication? I'm very stuck on that :(   regards Alex #lis331dlh

sam239955 by Associate II
  • 1387 Views
  • 2 replies
  • 0 kudos

STM32F103RB TIM1 INPUT CAPTURE QUESTION?

Posted on September 28, 2011 at 18:33hi, dear Frs.   now i want use the TIM1 ch1,ch2 to decode rf decoded . which is rf encode is diphase coded.  i use the PA8 use rf data stream input pin.  rf datarate is 9.6k.   now i step steps is as belows:stati...

0690X00000602j2QAA.jpg 0690X00000602ktQAA.jpg
taurus3g by Associate
  • 1058 Views
  • 1 replies
  • 0 kudos

STE100P Register dump

Posted on September 28, 2011 at 18:09I have got the address of the PHY on my board. The address is 7. Now the STM32 is able to communicate with the PHY. But the collision led is still blinking after the initialization. Here is the register dump:0   ...

Artur1 by Associate II
  • 532 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.