2011-10-01 9:45 AM
Hi everyone!
I have some problem with USART interrupt while receiving. RXNE bit clearing automatically by entering the interrupt without any actions, therefore software cannot detect character received event. I use STM32VL Discovery board, pins PB11 and PA9 is interconnected. // USART RXNE TEST #include ''stm32f10x.h'' vu8 n; u16 *ptr; u16 Buf[100]; void USART3_IRQHandler (void) { if(USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) { *ptr++ = USART_ReceiveData (USART3); // Never get here!!! } } void usart1_out (u16 data) { while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET) {;} USART_SendData(USART1, (u16)data); } int main(void) { USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; ErrorStatus HSEStartUpStatus; GPIO_InitTypeDef GPIO_InitStructure; u8 i; n=1; ptr=&Buf[0]; RCC_DeInit(); RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(RCC_HCLK_Div1) RCC_HSEConfig(RCC_HSE_ON); HSEStartUpStatus = RCC_WaitForHSEStartUp() if (HSEStartUpStatus == SUCCESS) { RCC_PREDIV1Config(RCC_PREDIV1_Source_HSE, RCC_PREDIV1_Div1);/* PLLCLK = (8MHz_ext/1) * 3 = 24 MHz */ RCC_PLLConfig(RCC_PLLSource_PREDIV1, RCC_PLLMul_3); }else{while(1){;}} RCC_PLLCmd(ENABLE); while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) {;} RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); while (RCC_GetSYSCLKSource() != 0x08) {;} NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); GPIO_DeInit (GPIOA); GPIO_DeInit (GPIOB); RCC_APB2PeriphClockCmd (RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd (RCC_APB2Periph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; /* Tx */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; /* Rx */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStructure); RCC_APB2PeriphClockCmd (RCC_APB2Periph_USART1, ENABLE); /* Configuring USART */ RCC_APB1PeriphClockCmd (RCC_APB1Periph_USART3, ENABLE); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); USART_InitStructure.USART_Mode = USART_Mode_Rx; USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE); USART_ITConfig(USART3, USART_IT_RXNE, ENABLE); while(1) { for (i=0; i<255; i++) { while (n==0){;} n=0; usart1_out (i); } } } This code doesn`t work on two different STM32VL discovery boards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.