STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Atollic TrueSTUDIO Lite: Is this a misprint?

Posted on October 09, 2011 at 18:32Hello everybody, Potential new user of ST chips here, feeling somewhat silly for asking this. However: Is the information provided by Atollic in their feature comparison document, v2.2, accurate? I am in particular...

Access to external memory during DMA transfer

Posted on January 09, 2012 at 10:44Hi all, my question is in direct relation with the AN3241 application note (TFT-LCD direct drive using the STM32F10xx FSMC peripheral). In the application note, two mode are possible (page 11, 2.4.1), ''slide show'...

TCP/IP socket

Posted on January 09, 2012 at 13:27Is it possible to have a ethernet port and open a socket port where a PC can send/receive a stream of data with the ARM processor? How should I do this? Do you have a tutorial/sample for me? Thank you #socket-et...

Where to download STM32 encryption library?

Posted on December 21, 2011 at 11:53Hi, i made a project to a customer with a STM32F102 and i will need to implement AES128. I Could read on a ST folder that there is available a STM32 encryption library to implement such algorithm. Where can i down...

luisf by Associate II
  • 1959 Views
  • 4 replies
  • 0 kudos

FAT32 problem stm32f205

Posted on November 30, 2011 at 08:45Hi Everybody,i m working on a project that needs data logging. I use FATFs ( Chan-FAT32 ) but i have a problem that described below:( I've formatted the SD card on PC with FAT32 )I try to create a .txt file, and c...

enturk by Associate II
  • 5801 Views
  • 17 replies
  • 0 kudos

FTP Client on STM32

Posted on January 07, 2012 at 22:09Hi All The following new video shows a demonstration of embedded FTP client operation in the uTasker project: http://youtu.be/sZOCFLDfGTk It is not shown running on an STM32 board in the demo but it is now included...

hpipon957 by Associate III
  • 2177 Views
  • 1 replies
  • 0 kudos

DCMI on STM32F4-Discovery board

Posted on January 08, 2012 at 22:49Can DCMI be used on the STM32F4Discovery board? It appears that there are pin conflicts that make it impossible.PA4 - DCMI_HSYNC conflicts with CS43L22 - LRCK/AN1xPA6 - DCMI_PIXCLK conflicts with LIS302DL - SDOPB6 ...

swenson by Associate
  • 807 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.