2011-12-21 2:53 AM
Hi, i made a project to a customer with a STM32F102 and i will need to implement AES128. I Could read on a ST folder that there is available a STM32 encryption library to implement such algorithm. Where can i download. If i need to request it, how can i make the request?
Thank you!2011-12-21 8:06 AM
I think you need to request through your local ST rep or FAE. If you don't have a contact point start with the regional sales office for your area/country.
''The AES-ECB 128-bit benchmark for the STM32 is available upon request''2011-12-22 1:44 PM
Thank you for your answer. As i could understand just the benchmark was available upon request. Anyway i will try to get in touch with them.
Thank you!2011-12-22 5:04 PM
Yeah, I think it's the library/demo/benchmark, others have asked after it in the past. There is probably paperwork involved.
There's plenty of generic AES source out there, although one of the speed improvements would to be putting the tables/code in SRAM. Competitors get some advantage by ROMing things (single cycle), instead of the 3 cycle hit from FLASH2012-01-09 1:26 AM
Hi,
Im trying to get encryption library. But i couldnt get the library by request. Did you get the library?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.