2012-01-07 1:09 PM
Hi All
The following new video shows a demonstration of embedded FTP client operation in the uTasker project: It is not shown running on an STM32 board in the demo but it is now included in the uTasker STM32 project as detailed here: It is therefore operational on STM32F1, STM32F2 and STM32F4 evaluation boards using GCC, Rowley Crossworks, ATOLLIC TrueStudio, IAR or Keil uVision, as well as in real-time simulation in VisualStudio 6 or VisualStudio 20xx. The FTP client user's manual is available at Regards Mark #utasker-stm32-ftp-client2012-01-09 12:00 AM
Very interesting.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.