2012-01-08 1:49 PM
Can DCMI be used on the STM32F4Discovery board? It appears that there are pin conflicts that make it impossible.
PA4 - DCMI_HSYNC conflicts with CS43L22 - LRCK/AN1xPA6 - DCMI_PIXCLK conflicts with LIS302DL - SDOPB6 - DCMI_D5 conflicts with CS43L22 - SCLPC7 - DCMI_D1 conflicts with CS43L22 - MCLKThe STM3240G-EVAL board appears to use the H and I pins to avoid these conflicts.For reference, I am looking at Table 5 of DM00039084.pdf (User Manual for STM32F4DISCOVERY) and Figure 20 of DM00036746.pdf (for the STM3240G-EVAL board). Any comments or suggestions? Thanks.2012-01-08 4:00 PM
Can DCMI be used on the STM32F4Discovery board? It appears that there are pin conflicts that make it impossible.Any comments or suggestions? Thanks.
Impossible seems to overstate the problem, it is a $15-20 USD board, remove the conflicting external hardware and experiment. It is classed as a ''throw away'' board with which to ''get creative'', if you need a more feature rich board it is likely an order of magnitude more expensive.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.