STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

pin VBUSON stm32-h107

Posted on April 02, 2012 at 22:40Hello to all, i have a question regarding stm32-h107 : in order to use feature usb on the go, should i connect pin USB_VBUSON to Vdd? Best Regards, Dion

dion by Associate II
  • 1333 Views
  • 2 replies
  • 0 kudos

Cannot for the life of me get TIM2 to trigger ADC1

Posted on April 03, 2012 at 08:00 Hi all, Bit at my wits end here. I have been trying for quite some time to get ADC1 to trigger on TIM2 CC2. To start with, I tried to use TIM3 TRGO with about the same amount of luck (ie none). Everything...

jeremyh by Associate II
  • 724 Views
  • 0 replies
  • 0 kudos

STM32F100RC -- GPIO in standby mode

Posted on March 31, 2012 at 12:02What is the state of GPIO pins when microcontroller is in standby mode?  Each pin remembers it's own state: input, output, analog, pull-up, logic level on it?  Which document (datasheet, etc) and where specifies this...

sysop by Associate II
  • 2196 Views
  • 4 replies
  • 0 kudos

Failed to load flash loader with STM32F4 Discovery

Posted on March 31, 2012 at 23:17Hello, I am using STM32F4 Discovery for a DSP project at my University. The professor uses the previous version of Discovery with the Cortex-M3. When I tried running his project on my board I get the following messag...

dfranch6 by Associate
  • 1906 Views
  • 2 replies
  • 0 kudos

EXTIn: n > 4

Posted on March 29, 2012 at 07:30I have one external interrupt working fine, but I need to add a few more and I'm failing to understand how it all maps out.The one I have implemented is on PA3 and the ISR is void EXTI3_IRQHandler(void). Although the...

cmcquaid by Associate
  • 943 Views
  • 2 replies
  • 0 kudos

Prescaler and timers

Posted on March 30, 2012 at 10:17How can I configurethePort Aprescalerto readevery 5seconds.What is theformulathat is used?Is there adocument that explains howI setthe timers?

eixp12 by Associate II
  • 1984 Views
  • 4 replies
  • 0 kudos

STM32 Pulse Counter

Posted on March 28, 2012 at 17:29I wonder if someone could help me. I want to count the number of pulses occured each ''x'' time. I could use a timer configured to generate an interrupt each ''x'' time. And the interrupt handler of this timer shou...

tecnico23 by Associate II
  • 4738 Views
  • 19 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.