2012-04-02 1:40 PM
Hello to all,
i have a question regarding stm32-h107 : in order to use feature usb on the go, should i connect pin USB_VBUSON to Vdd? Best Regards, Dion2012-04-02 9:28 PM
Better refer to Evaluation board schematics.
The VBus needs to be connected to the USB Power Switch output and also to Vbus of the STM32F105. The Power switch is needed for using the MCU in host mode and direct connection to Vbus is needed to use in device mode. The Power-switch enable needs to be controlled by mcu.2012-04-03 12:45 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.