STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A few questions on the STM32L...

Posted on April 09, 2012 at 18:46 Is there a proper way to go into low-power sleep? When I try to step through in the debugger (or at least, let the program run and then pause it), the LPSDSR flag never gets set. And when I let the program run wit...

shotaro by Associate II
  • 1688 Views
  • 7 replies
  • 0 kudos

Proper way to switch to HSE

Posted on April 05, 2012 at 18:43My application calls for using an external oscillator (not a crystal) as a clock source. To test this, I have an arbitrary function generator outputting a 50% duty cycle square wave of the expected clock rate. The MC...

shotaro by Associate II
  • 2375 Views
  • 3 replies
  • 0 kudos

STM32L151 jtag problem

Posted on April 08, 2012 at 16:18Hello ! I I start working with STM32L151  + Keil + ULINK2 ,  and  met a problem : after some code,  likely  it was  scommand  GPIOA->BSRRL=GPIO_BSRR_BS_2;processor stop the debugging, and a can not start  a new debu...

delay from two signals

Posted on April 03, 2012 at 20:12Hello at all, I have to mesaure the delay between 2 signals that I have in input to the microcontroller. I saw the example of the PWM input. I supposed to use an OR gate to have both front to the same pin but I think...

momede by Associate II
  • 2686 Views
  • 5 replies
  • 0 kudos

ST32F217 with STE100P. How to configure PHY address?

Posted on April 04, 2012 at 07:04STE100P how to set PHY address?Hello. Im trying to using an STE100P PHY ethernet chip (with ST32F217 MCU). In the datasheet for STE100P i see an description for bits 7~3 PAD4:0 in PR20- XMC, XCVR Mode control registe...

andrey23 by Associate II
  • 2375 Views
  • 4 replies
  • 0 kudos

Ethernet PHY DP83848CVV

Posted on April 04, 2012 at 13:55Hello, I want to use DP83848CVV as Ethenet PHY with STM32F207ZET6 in RMII mode. In Schematics (STM3220G_EVAL),there is some resistor of 51 Ohm in between of  signals (RMII_REF_CLK,RMII_TX_EN,RMII_TX_D0,RMII_TX_D1,RMI...

migrating from Atollic to IAR

Posted on April 05, 2012 at 07:39Hello, reasently i changed ide to iar and i getting strange problems: i have working code developed in atollic and tested on my discovery boards, but then i use same code on IAR, it just doesn't work. Like touchscre...

linas2 by Associate II
  • 1737 Views
  • 3 replies
  • 0 kudos

STM32F207

Posted on April 04, 2012 at 12:16Hello, I would like to download a C compiler for STM32F207. Where I could find it? I was searching through the forum, but without success. #stm32f207 #c/c++-compiler

dove457 by Associate
  • 1512 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.