2012-04-03 4:44 AM
Hello all.
I need to quickly learn how to use the Ethernet on the STM32F217 MCU. 1. I need to be able to setup a webpage that is shown with on board measurements. 2. I must also be able to download and upload data/files to the MCU. (FTP or other)And what about the RMII and MII, what do I select? I assume that there are a lot of different transceivers for that?Do I need some kind of driver for the selected transceiver? Where do I start?2012-04-03 5:39 AM
Dear SirM:
It looks your situation very like me.I suggest try to use STM sample code to learn it will more quickly. I didn't know the MII or RMII also. But I try to keep learn and do it at the same time.I am also very grateful to the help of my friends in this forum.
http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32f2x7_eth_lwip.zip
Hope these can help you.Simon2012-04-03 7:53 AM
Perhaps you could get some boards with the 207/Ethernet already functioning and replace with a 217 part. ie start with something known to work, before getting creative with your own part selections.
http://www.olimex.com/dev/stm32-p207.html
2012-04-03 11:59 PM
I received an olimex STM32-P207 board yesterday. The 207 is very similar to the 217 (I think). So I can begin to understand and test the Ethernet.
One more question. Is it possible to generate a 50MHz RMII clock with the MCU?2012-04-04 5:50 AM
My understanding is the difference between the 207/217 is the availability of the HASH/CRYPTO block. There are a number of variants which share a common footprint.
Getting 25 MHz out should be easy enough, using an external 25 MHz crystal. I suspect you can get 50 MHz out with a clever/suboptimal selection of a clocking plan. ie running the core at 100 MHz. You could also use a single 50 MHz external clock, and divide that down to run the STM32F22012-04-05 4:23 AM
Hello,
For RMII mode, you have to provide the 50 MHz clock by soldering a 50 MHz oscillator (ref SM7745HEV-50.0M or equivalent) on the U3 footprint located under CN3 and also removing jumper on JP5. This oscillator is not provided with the board. For more details, please refer to STM3220G-EVAL evaluation board User manual (UM1057).2012-04-05 9:20 AM
For RMII mode, you have to provide the 50 MHz clock by soldering a 50 MHz oscillator (ref SM7745HEV-50.0M or equivalent) on the U3 footprint located under CN3 and also removing jumper on JP5. This oscillator is not provided with the board. For more details, please refer to STM3220G-EVAL evaluation board User manual (UM1057).
On his board CD1 (50 MHz) appears to be populated, at least in the web page picture. Should be able to push PLL/2 out of MCO1, or MCO2, when running the CPU at 100 MHz (ie 25 MHZ x 4, or 10 MHz x 10), can't say if the PLL generates a nice clock
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.